Structure to hold the parameters of the SYSRTC clock-source configurations.

This structure contains the configuration parameters for the SYSRTC clock source. It includes the clock source and the division factor.

Public Attributes#

uint8_t

Input clock source from sl_clock_sources_t (clock sources enum)

uint32_t

Clock division factor.

Public Attribute Documentation#

clock_source#

uint8_t sl_sysrtc_clock_config_t::clock_source

Input clock source from sl_clock_sources_t (clock sources enum)


Definition at line 105 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

division_factor#

uint32_t sl_sysrtc_clock_config_t::division_factor

Clock division factor.


Definition at line 106 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h