Structure to hold the parameters for SYSRTC group interrupt enabling bits.

This structure contains the configuration parameters for enabling or disabling interrupts for SYSRTC groups. Each member represents whether a specific interrupt type is enabled (true) or disabled (false).

Public Attributes#

boolean_t

true to enable group 0 overflow interrupt, false to disable it

boolean_t

true to enable group 0 compare 0 interrupt, false to disable it

boolean_t

true to enable group 0 compare 1 interrupt, false to disable it

boolean_t

true to enable group 0 capture 0 interrupt, false to disable it

boolean_t

true to enable group 1 overflow interrupt, false to disable it

boolean_t

true to enable group 1 compare 0 interrupt, false to disable it

boolean_t

true to enable group 1 compare 1 interrupt, false to disable it

boolean_t

true to enable group 1 capture 0 interrupt, false to disable it

Public Attribute Documentation#

group0_overflow_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group0_overflow_interrupt_is_enabled

true to enable group 0 overflow interrupt, false to disable it


Definition at line 117 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group0_compare0_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group0_compare0_interrupt_is_enabled

true to enable group 0 compare 0 interrupt, false to disable it


Definition at line 118 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group0_compare1_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group0_compare1_interrupt_is_enabled

true to enable group 0 compare 1 interrupt, false to disable it


Definition at line 119 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group0_capture0_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group0_capture0_interrupt_is_enabled

true to enable group 0 capture 0 interrupt, false to disable it


Definition at line 120 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group1_overflow_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group1_overflow_interrupt_is_enabled

true to enable group 1 overflow interrupt, false to disable it


Definition at line 121 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group1_compare0_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group1_compare0_interrupt_is_enabled

true to enable group 1 compare 0 interrupt, false to disable it


Definition at line 122 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group1_compare1_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group1_compare1_interrupt_is_enabled

true to enable group 1 compare 1 interrupt, false to disable it


Definition at line 123 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

group1_capture0_interrupt_is_enabled#

boolean_t sl_sysrtc_interrupt_enables_t::group1_capture0_interrupt_is_enabled

true to enable group 1 capture 0 interrupt, false to disable it


Definition at line 124 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h