Structure representing the BLE command to update connection parameters.

This structure is used to define the parameters for a BLE command to update connection parameters, including the address of the connected device, minimum and maximum connection intervals, peripheral latency, and supervision timeout.

Public Attributes#

uint8_t

Address of the connected device.

uint16_t

Minimum connection interval.

uint16_t

Maximum connection interval.

uint16_t

Peripheral latency.

uint16_t

Supervision timeout.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_cmd_conn_params_update_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the connected device.


min_interval#

uint16_t rsi_ble_cmd_conn_params_update_s::min_interval

Minimum connection interval.


max_interval#

uint16_t rsi_ble_cmd_conn_params_update_s::max_interval

Maximum connection interval.


latency#

uint16_t rsi_ble_cmd_conn_params_update_s::latency

Peripheral latency.


timeout#

uint16_t rsi_ble_cmd_conn_params_update_s::timeout

Supervision timeout.