Structure representing the BLE request to set PHY.

This structure is used to define the parameters for a BLE request to set the PHY, including the address of the connected device, all PHYs preference, preferred TX PHY, preferred RX PHY, reserved field for future use, and PHY options.

Public Attributes#

uint8_t

Address of the connected device.

uint8_t

All PHYs preference.

uint8_t

Preferred TX PHY.

uint8_t

Preferred RX PHY.

uint8_t

Reserved for future use.

uint16_t

PHY options.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_set_phy_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the connected device.


all_phy#

uint8_t rsi_ble_set_phy_s::all_phy

All PHYs preference.


tx_phy#

uint8_t rsi_ble_set_phy_s::tx_phy

Preferred TX PHY.


rx_phy#

uint8_t rsi_ble_set_phy_s::rx_phy

Preferred RX PHY.


reserved#

uint8_t rsi_ble_set_phy_s::reserved

Reserved for future use.


phy_options#

uint16_t rsi_ble_set_phy_s::phy_options

PHY options.