Structure representing the BLE notification for an attribute value.

This structure is used to define the parameters for a BLE notification of an attribute value, including the remote device address, the attribute handle, the length of the attribute value, and the attribute value itself.

Public Attributes#

uint8_t

Remote device address.

uint16_t

Attribute handle.

uint16_t

Attribute value length.

uint8_t

Attribute value (data)

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_notify_att_value_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


handle#

uint16_t rsi_ble_notify_att_value_s::handle

Attribute handle.


data_len#

uint16_t rsi_ble_notify_att_value_s::data_len

Attribute value length.


data#

uint8_t rsi_ble_notify_att_value_s::data[RSI_DEV_ATT_LEN]

Attribute value (data)