Structure representing the BLE request to enable or disable address resolution.

This structure is used to define the parameters for a BLE request to enable or disable address resolution, including the enable flag, reserved field for future use, and the timeout value for address resolution.

Public Attributes#

uint8_t

Enable or disable address resolution.

uint8_t

Reserved for future use.

uint16_t

Timeout value for address resolution.

Public Attribute Documentation#

enable#

uint8_t rsi_ble_set_addr_resolution_enable_s::enable

Enable or disable address resolution.


reserved#

uint8_t rsi_ble_set_addr_resolution_enable_s::reserved

Reserved for future use.


tout#

uint16_t rsi_ble_set_addr_resolution_enable_s::tout

Timeout value for address resolution.