Possible Error Codes#

Command

Error Code

Description

Cause of failure

MBR

0xa0ac

Verification failed from flash

There may be a wrong input from the user to select pinset/damaged MBR file

Activation code

0xa0b0

Activation code generated failed

security module might throw an error if PUF enroll fails, if the device is locked to use PUF

Intrinsic keys

0xa0b1

Intrinsic keys generation failed

This may occur if this command triggered before activation code command.

Static keys

0xa0b2

Static keys stored failed

This may occur if there are no intrinsic keys.

Update Firmware

108

Failed to load firmware

This may occur if the header part of rps file is not proper.