LFN connection parameters.
Public Attributes#
uint8_t
Duration of LFN PAN Advertisement (LPA) listening slot (millisecond) Specification range [15, 255].
uint8_t
Number of LPA slots for which an LFN shall listen for LPA frames Specification range [1, 255].
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
discovery_slot_time_ms#
uint8_t sl_wisun_lfn_params_connection_t::discovery_slot_time_ms
Duration of LFN PAN Advertisement (LPA) listening slot (millisecond) Specification range [15, 255].
Definition at line
52
of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
discovery_slots#
uint8_t sl_wisun_lfn_params_connection_t::discovery_slots
Number of LPA slots for which an LFN shall listen for LPA frames Specification range [1, 255].
Definition at line
55
of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
reserved#
uint8_t sl_wisun_lfn_params_connection_t::reserved[2]
Reserved, set to zero.
Definition at line
57
of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h