RPL parameter set.

Public Attributes#

uint16_t

RPL first DIS maximum delay (seconds)

uint16_t

RPL DIS maximum delay (seconds)

uint16_t

Delay for preferred parent selection after first DIO reception (seconds)

uint16_t

Maximum period of NS probes used to get samples for ETX calculation (seconds)

uint8_t

Number of samples used to calculate ETX during join state 4.

uint8_t

Number of samples used to refresh ETX.

uint8_t

RPL max candidate parents.

uint8_t

RPL max parents.

Public Attribute Documentation#

dis_max_delay_first_s#

uint16_t sl_wisun_params_rpl::dis_max_delay_first_s

RPL first DIS maximum delay (seconds)


Definition at line 137 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

dis_max_delay_s#

uint16_t sl_wisun_params_rpl::dis_max_delay_s

RPL DIS maximum delay (seconds)


Definition at line 139 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

init_parent_selection_s#

uint16_t sl_wisun_params_rpl::init_parent_selection_s

Delay for preferred parent selection after first DIO reception (seconds)


Definition at line 141 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

etx_probe_period_max_s#

uint16_t sl_wisun_params_rpl::etx_probe_period_max_s

Maximum period of NS probes used to get samples for ETX calculation (seconds)


Definition at line 143 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

etx_samples_init#

uint8_t sl_wisun_params_rpl::etx_samples_init

Number of samples used to calculate ETX during join state 4.


Definition at line 145 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

etx_samples_refresh#

uint8_t sl_wisun_params_rpl::etx_samples_refresh

Number of samples used to refresh ETX.


Definition at line 147 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

candidate_parents_max#

uint8_t sl_wisun_params_rpl::candidate_parents_max

RPL max candidate parents.


Definition at line 149 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

parents_max#

uint8_t sl_wisun_params_rpl::parents_max

RPL max parents.


Definition at line 151 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h