Wi-SUN Message API common header.

Public Attributes#

uint16_t

Total length of the message in bytes, this field included.

uint8_t

ID (request, confirmation, indication) of the message.

uint8_t

Processing metadata for the message.

Public Attribute Documentation#

length#

uint16_t sl_wisun_msg_header_t::length

Total length of the message in bytes, this field included.


Definition at line 327 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

id#

uint8_t sl_wisun_msg_header_t::id

ID (request, confirmation, indication) of the message.


Definition at line 329 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

info#

uint8_t sl_wisun_msg_header_t::info

Processing metadata for the message.


Definition at line 331 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h