Misc parameter set.

Public Attributes#

uint16_t

Temporary neighbor link minimum timeout.

uint8_t

Border router communication timeout PAN_TIMEOUT.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

temp_link_min_timeout_s#

uint16_t sl_wisun_params_misc::temp_link_min_timeout_s

Temporary neighbor link minimum timeout.


Definition at line 173 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

pan_timeout_m#

uint8_t sl_wisun_params_misc::pan_timeout_m

Border router communication timeout PAN_TIMEOUT.


Definition at line 175 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

reserved#

uint8_t sl_wisun_params_misc::reserved

Reserved, set to zero.


Definition at line 177 of file /mnt/raid/workspaces/ws.XvhINl85J/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h