LFN data layer parameters.

Public Attributes#

uint32_t

Time between LFN sampled listening points (milliseconds)

uint32_t

Minimum acceptable LFN unicast interval (milliseconds)

uint32_t

Maximum acceptable LFN unicast interval (milliseconds)

uint8_t

The number of LFN Broadcast Sync Period (parent defined) after which, having not received any messaging from its parent, an LFN assumes the parent is lost.

Public Attribute Documentation#

unicast_interval_ms#

uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_ms

Time between LFN sampled listening points (milliseconds)


unicast_interval_min_ms#

uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_min_ms

Minimum acceptable LFN unicast interval (milliseconds)


unicast_interval_max_ms#

uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_max_ms

Maximum acceptable LFN unicast interval (milliseconds)


lfn_maintain_parent_time#

uint8_t sl_wisun_lfn_params_data_layer_t::lfn_maintain_parent_time

The number of LFN Broadcast Sync Period (parent defined) after which, having not received any messaging from its parent, an LFN assumes the parent is lost.

Specification range [1, 60]