PAN discovery parameter set.

Public Attributes#

PAN Advertisement trickle timer.

PAN Advertisement Solicit trickle timer.

uint8_t

Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.

bool

If true, allow join state 1 to be skipped using cached information from the previous connection.

Public Attribute Documentation#

trickle_pa#

sl_wisun_trickle_params_t sl_wisun_params_discovery::trickle_pa

PAN Advertisement trickle timer.


trickle_pas#

sl_wisun_trickle_params_t sl_wisun_params_discovery::trickle_pas

PAN Advertisement Solicit trickle timer.


eapol_target_min_sens#

uint8_t sl_wisun_params_discovery::eapol_target_min_sens

Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.

Range from -174 (0) to +80 (254) dBm, 255 to disable feature.


allow_skip#

bool sl_wisun_params_discovery::allow_skip

If true, allow join state 1 to be skipped using cached information from the previous connection.