LFN power parameters.

Public Attributes#

uint16_t

Minimum sampled listen width (microseconds) Sampled listen is calculated with PHY parameters.

uint16_t

Minimum listening window margin (microseconds) Window Margin is calculated dynamically with aging synchronization info.

bool

If true, the node limits LFN broadcast interval wakeups to minimum while still maintaining time synchronization with the parent.

Public Attribute Documentation#

listening_window_min_us#

uint16_t sl_wisun_lfn_params_power_t::listening_window_min_us

Minimum sampled listen width (microseconds) Sampled listen is calculated with PHY parameters.

Set to force sampled listen duration above this value.


Definition at line 96 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

window_margin_min_us#

uint16_t sl_wisun_lfn_params_power_t::window_margin_min_us

Minimum listening window margin (microseconds) Window Margin is calculated dynamically with aging synchronization info.

Set to force margin above this value.


Definition at line 100 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

broadcast_lts_only#

bool sl_wisun_lfn_params_power_t::broadcast_lts_only

If true, the node limits LFN broadcast interval wakeups to minimum while still maintaining time synchronization with the parent.

If false, the node wakes up on every LFN broadcast interval.


Definition at line 104 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h