Predefined BR LFN-parenting parameter sets#

Predefined LFN parameter sets for sl_wisun_br_set_lfn_parameters().

These parameter sets can be used either as-is or used as an initialization value for an application-specific parameter set.

Variables#

Profile providing balance between battery life and performance.

Profile with a higher battery life.

Profile for use during tests.

Variable Documentation#

SL_WISUN_BR_PARAMS_LFN_BALANCED#

const sl_wisun_br_lfn_params_t SL_WISUN_BR_PARAMS_LFN_BALANCED

Profile providing balance between battery life and performance.


Definition at line 89 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_lfn_params_api.h

SL_WISUN_BR_PARAMS_LFN_ECO#

const sl_wisun_br_lfn_params_t SL_WISUN_BR_PARAMS_LFN_ECO

Profile with a higher battery life.


Definition at line 97 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_lfn_params_api.h

SL_WISUN_BR_PARAMS_LFN_TEST#

const sl_wisun_br_lfn_params_t SL_WISUN_BR_PARAMS_LFN_TEST

Profile for use during tests.


Definition at line 81 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_lfn_params_api.h