PAN discovery parameter set.
Public Attributes#
uint8_t
If true, allow join state 1 to be skipped using cached information from the previous connection.
uint8_t
Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.
uint8_t
Reserved, set to zero.
PAN Advertisement trickle timer.
PAN Advertisement Solicit trickle timer.
Public Attribute Documentation#
allow_skip#
uint8_t sl_wisun_params_discovery_s::allow_skip
If true, allow join state 1 to be skipped using cached information from the previous connection.
Definition at line
124
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
eapol_target_min_sens#
uint8_t sl_wisun_params_discovery_s::eapol_target_min_sens
Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.
Range from -174 (0) to +80 (254) dBm, 255 to disable feature.
Definition at line
121
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
reserved#
uint8_t sl_wisun_params_discovery_s::reserved[2]
Reserved, set to zero.
Definition at line
126
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
trickle_pa#
sl_wisun_trickle_params_t sl_wisun_params_discovery_s::trickle_pa
PAN Advertisement trickle timer.
Definition at line
115
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
trickle_pas#
sl_wisun_trickle_params_t sl_wisun_params_discovery_s::trickle_pas
PAN Advertisement Solicit trickle timer.
Definition at line
117
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h