BR parameter set.

Public Attributes#

PAN configuration parameter set.

DHCP server parameter set.

PAN discovery parameter set.

Authentication parameter set.

uint8_t

Enable authentication of FAN 1.0 routers.

Misc parameter set.

MPL parameter set.

uint32_t

Maximum number of nodes supported by border router at once.

uint8_t

Reserved, set to zero.

RPL parameter set.

uint32_t

Version of this API.

Public Attribute Documentation#

configuration#

sl_wisun_br_params_configuration_t sl_wisun_br_connection_params_t::configuration

PAN configuration parameter set.


dhcp#

sl_wisun_br_params_dhcp_t sl_wisun_br_connection_params_t::dhcp

DHCP server parameter set.


discovery#

sl_wisun_br_params_discovery_t sl_wisun_br_connection_params_t::discovery

PAN discovery parameter set.


eapol#

sl_wisun_br_params_eapol_t sl_wisun_br_connection_params_t::eapol

Authentication parameter set.


enable_ffn10#

uint8_t sl_wisun_br_connection_params_t::enable_ffn10

Enable authentication of FAN 1.0 routers.


lfn_parent#

sl_wisun_br_params_lfn_parent_t sl_wisun_br_connection_params_t::lfn_parent

LFN parent parameter set.


misc#

sl_wisun_br_params_misc_t sl_wisun_br_connection_params_t::misc

Misc parameter set.


mpl#

sl_wisun_br_params_mpl_t sl_wisun_br_connection_params_t::mpl

MPL parameter set.


pan_capacity#

uint32_t sl_wisun_br_connection_params_t::pan_capacity

Maximum number of nodes supported by border router at once.


reserved#

uint8_t sl_wisun_br_connection_params_t::reserved[3]

Reserved, set to zero.


rpl#

sl_wisun_br_params_rpl_t sl_wisun_br_connection_params_t::rpl

RPL parameter set.


version#

uint32_t sl_wisun_br_connection_params_t::version

Version of this API.

This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.