Authentication parameter set.
Public Attributes#
If true, allow join state 2 to be skipped using cached credentials from the previous connection.
GTK_MAX_MISMATCH (minutes)
GTK_REQUEST_IMAX (minutes)
GTK_REQUEST_IMIN (minutes)
Initial EAPOL-Key first Tx max delay (seconds)
Initial EAPOL-Key first Tx min delay (seconds)
Initial EAPOL-Key retry limit.
Initial EAPOL-Key retry exponential backoff max limit (seconds)
Initial EAPOL-Key retry exponential backoff max (seconds)
Initial EAPOL-Key retry exponential backoff min (seconds)
LGTK_MAX_MISMATCH (minutes)
PMK lifetime (minutes)
PTK lifetime (minutes)
Reserved, set to zero.
Security protocol retry timeout (seconds)
Security protocol trickle timer.
Security protocol trickle timer expirations.
Temporary neighbor link minimum timeout (seconds)
Public Attribute Documentation#
allow_skip#
uint8_t sl_wisun_params_eapol_s::allow_skip
If true, allow join state 2 to be skipped using cached credentials from the previous connection.
initial_key_max_s#
uint16_t sl_wisun_params_eapol_s::initial_key_max_s
Initial EAPOL-Key first Tx max delay (seconds)
initial_key_min_s#
uint16_t sl_wisun_params_eapol_s::initial_key_min_s
Initial EAPOL-Key first Tx min delay (seconds)
initial_key_retry_limit#
uint8_t sl_wisun_params_eapol_s::initial_key_retry_limit
Initial EAPOL-Key retry limit.
initial_key_retry_max_limit_s#
uint16_t sl_wisun_params_eapol_s::initial_key_retry_max_limit_s
Initial EAPOL-Key retry exponential backoff max limit (seconds)
initial_key_retry_max_s#
uint16_t sl_wisun_params_eapol_s::initial_key_retry_max_s
Initial EAPOL-Key retry exponential backoff max (seconds)
initial_key_retry_min_s#
uint16_t sl_wisun_params_eapol_s::initial_key_retry_min_s
Initial EAPOL-Key retry exponential backoff min (seconds)
lgtk_max_mismatch_m#
uint16_t sl_wisun_params_eapol_s::lgtk_max_mismatch_m
LGTK_MAX_MISMATCH (minutes)
sec_prot_retry_timeout_s#
uint16_t sl_wisun_params_eapol_s::sec_prot_retry_timeout_s
Security protocol retry timeout (seconds)
sec_prot_trickle#
sl_wisun_trickle_params_t sl_wisun_params_eapol_s::sec_prot_trickle
Security protocol trickle timer.
sec_prot_trickle_expirations#
uint8_t sl_wisun_params_eapol_s::sec_prot_trickle_expirations
Security protocol trickle timer expirations.
temp_min_timeout_s#
uint16_t sl_wisun_params_eapol_s::temp_min_timeout_s
Temporary neighbor link minimum timeout (seconds)