LFN parent parameter set.

Public Attributes#

uint8_t

Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.

uint8_t

Duration for which an FFN retransmits DAO on behalf of a registering LFN (minutes).

uint16_t

Interval after which an FFN parent must disable LFN broadcast messaging if the FFN parent is unable communicate with its Border Router.

Public Attribute Documentation#

lfn_lpc_retry_count#

uint8_t sl_wisun_params_lfn_parent_s::lfn_lpc_retry_count

Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.


lfn_na_wait_duration_m#

uint8_t sl_wisun_params_lfn_parent_s::lfn_na_wait_duration_m

Duration for which an FFN retransmits DAO on behalf of a registering LFN (minutes).

This value is administratively configured and should be consistent throughout the network. Make sure that the value is equal to or less than the corresponding field on LFNs. Specification range [30, 120] (set lower for test purposes)


lfn_pan_timeout_m#

uint16_t sl_wisun_params_lfn_parent_s::lfn_pan_timeout_m

Interval after which an FFN parent must disable LFN broadcast messaging if the FFN parent is unable communicate with its Border Router.