RPL parameter set.
Public Attributes#
Amount of time a parent should retain a registered GUA/ULA (seconds)
RPL max candidate parents.
RPL first DIS maximum delay (seconds)
RPL DIS maximum delay (seconds)
Maximum period of NS probes used to get samples for ETX calculation (seconds)
Number of samples used to calculate ETX during join state 4.
Number of samples used to refresh ETX.
Delay for preferred parent selection after first DIO reception (seconds)
RPL max parents.
Public Attribute Documentation#
address_registration_lifetime_s#
uint16_t sl_wisun_params_rpl_s::address_registration_lifetime_s
Amount of time a parent should retain a registered GUA/ULA (seconds)
candidate_parents_max#
uint8_t sl_wisun_params_rpl_s::candidate_parents_max
RPL max candidate parents.
dis_max_delay_first_s#
uint16_t sl_wisun_params_rpl_s::dis_max_delay_first_s
RPL first DIS maximum delay (seconds)
etx_probe_period_max_s#
uint16_t sl_wisun_params_rpl_s::etx_probe_period_max_s
Maximum period of NS probes used to get samples for ETX calculation (seconds)
etx_samples_init#
uint8_t sl_wisun_params_rpl_s::etx_samples_init
Number of samples used to calculate ETX during join state 4.
etx_samples_refresh#
uint8_t sl_wisun_params_rpl_s::etx_samples_refresh
Number of samples used to refresh ETX.
init_parent_selection_s#
uint16_t sl_wisun_params_rpl_s::init_parent_selection_s
Delay for preferred parent selection after first DIO reception (seconds)