PAN discovery parameter set.
Public Attributes#
uint8_t
If true, allow join state 1 to be skipped using cached information from the previous connection.
uint8_t
Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.
uint8_t
Reserved, set to zero.
PAN Advertisement trickle timer.
PAN Advertisement Solicit trickle timer.
Public Attribute Documentation#
allow_skip#
uint8_t sl_wisun_params_discovery_s::allow_skip
If true, allow join state 1 to be skipped using cached information from the previous connection.
eapol_target_min_sens#
uint8_t sl_wisun_params_discovery_s::eapol_target_min_sens
Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.
Range from -174 (0) to +80 (254) dBm, 255 to disable feature.
trickle_pa#
sl_wisun_trickle_params_t sl_wisun_params_discovery_s::trickle_pa
PAN Advertisement trickle timer.
trickle_pas#
sl_wisun_trickle_params_t sl_wisun_params_discovery_s::trickle_pas
PAN Advertisement Solicit trickle timer.