Key lifetimes parameter set.
Public Attributes#
FFN_REVOCATION_LIFETIME_REDUCTION Factor by which the active GTK lifetime is reduced during node revocation procedures.
GTK_EXPIRE_OFFSET (minutes) The expiration time of a GTK is calculated as the expiration time of the GTK most recently installed at the Border Router plus GTK_EXPIRE_OFFSET.
GTK_NEW_ACTIVATION_TIME The time at which the Border Router activates the next GTK prior to expiration of the currently activated GTK.
GTK_NEW_INSTALL_REQUIRED The percentage of time elapsed in the active GTK’s lifetime at which a new GTK must be installed on the Border Router.
LFN_REVOCATION_LIFETIME_REDUCTION Factor by which the active LGTK lifetime is reduced during node revocation procedures.
LGTK_EXPIRE_OFFSET (minutes) The expiration time of a LGTK is calculated as the expiration time of the GTK most recently installed at the Border Router plus LGTK_EXPIRE_OFFSET.
LGTK_NEW_ACTIVATION_TIME The time at which the Border Router activates the next LGTK prior to expiration of the currently activated LGTK.
LGTK_NEW_INSTALL_REQUIRED The percentage of time elapsed in the active LGTK’s lifetime at which a new LGTK must be installed on the Border Router.
LPMK lifetime (minutes)
LPTK lifetime (minutes)
PMK lifetime (minutes)
PTK lifetime (minutes)
Reserved, set to zero.
Public Attribute Documentation#
ffn_revocation_lifetime_reduction#
uint32_t sl_wisun_key_lifetimes_params_t::ffn_revocation_lifetime_reduction
FFN_REVOCATION_LIFETIME_REDUCTION Factor by which the active GTK lifetime is reduced during node revocation procedures.
gtk_expire_offset_m#
uint32_t sl_wisun_key_lifetimes_params_t::gtk_expire_offset_m
GTK_EXPIRE_OFFSET (minutes) The expiration time of a GTK is calculated as the expiration time of the GTK most recently installed at the Border Router plus GTK_EXPIRE_OFFSET.
gtk_new_activation_time#
uint32_t sl_wisun_key_lifetimes_params_t::gtk_new_activation_time
GTK_NEW_ACTIVATION_TIME The time at which the Border Router activates the next GTK prior to expiration of the currently activated GTK.
gtk_new_install_required#
uint32_t sl_wisun_key_lifetimes_params_t::gtk_new_install_required
GTK_NEW_INSTALL_REQUIRED The percentage of time elapsed in the active GTK’s lifetime at which a new GTK must be installed on the Border Router.
lfn_revocation_lifetime_reduction#
uint32_t sl_wisun_key_lifetimes_params_t::lfn_revocation_lifetime_reduction
LFN_REVOCATION_LIFETIME_REDUCTION Factor by which the active LGTK lifetime is reduced during node revocation procedures.
lgtk_expire_offset_m#
uint32_t sl_wisun_key_lifetimes_params_t::lgtk_expire_offset_m
LGTK_EXPIRE_OFFSET (minutes) The expiration time of a LGTK is calculated as the expiration time of the GTK most recently installed at the Border Router plus LGTK_EXPIRE_OFFSET.
lgtk_new_activation_time#
uint32_t sl_wisun_key_lifetimes_params_t::lgtk_new_activation_time
LGTK_NEW_ACTIVATION_TIME The time at which the Border Router activates the next LGTK prior to expiration of the currently activated LGTK.
lgtk_new_install_required#
uint32_t sl_wisun_key_lifetimes_params_t::lgtk_new_install_required
LGTK_NEW_INSTALL_REQUIRED The percentage of time elapsed in the active LGTK’s lifetime at which a new LGTK must be installed on the Border Router.