Wisun Event information.

Public Attributes#

Address of the node.

uint64_t

Event type.

union sl_wisun_logger_event_t::@5

Public Attribute Documentation#

address#

sl_wisun_mac_address_t sl_wisun_logger_event_t::address

Address of the node.


frame_received#

sl_wisun_logger_event_frame_received_t sl_wisun_logger_event_t::frame_received

Frame received information.


neighbor_lifetime_changed#

sl_wisun_logger_event_neighbor_lifetime_changed_t sl_wisun_logger_event_t::neighbor_lifetime_changed

Neighbor lifetime change information.


tx_failure#

sl_wisun_logger_event_tx_failure_t sl_wisun_logger_event_t::tx_failure

TX failure information.


type#

uint64_t sl_wisun_logger_event_t::type

Event type.


u#

union sl_wisun_logger_event_t::@5 sl_wisun_logger_event_t::u