Defines the different types that a value can take, e.g.

uint8_t, int16_t, etc.

Public Attributes#

uint32_t
uint16_t
uint8_t
int32_t
int16_t
int8_t

Public Attribute Documentation#

as_uint32#

uint32_t cc_config_parameter_value_t::as_uint32

Definition at line 66 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

as_uint16#

uint16_t cc_config_parameter_value_t::as_uint16

Definition at line 67 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

as_uint8#

uint8_t cc_config_parameter_value_t::as_uint8

Definition at line 68 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

as_int32#

int32_t cc_config_parameter_value_t::as_int32

Definition at line 70 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

as_int16#

int16_t cc_config_parameter_value_t::as_int16

Definition at line 71 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

as_int8#

int8_t cc_config_parameter_value_t::as_int8

Definition at line 72 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

as_uint8_array#

uint8_t cc_config_parameter_value_t::as_uint8_array[4]

Definition at line 74 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h