Holds a write and a read interface defined by the user.
Public Attributes#
bool(*
Write function which writes data with a specified size to non volatile memory.
bool(*
Read function which reads data with specified size from non volatile memory.
Public Attribute Documentation#
write_handler#
bool(* cc_configuration_io_interface_t::write_handler) (zpal_nvm_object_key_t file_id, uint8_t const *data, size_t size)
Write function which writes data with a specified size to non volatile memory.
Definition at line
133
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
read_handler#
bool(* cc_configuration_io_interface_t::read_handler) (zpal_nvm_object_key_t file_id, uint8_t *data, size_t size)
Read function which reads data with specified size from non volatile memory.
Definition at line
134
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h