a struct containing the superset of values passed to both emberIncomingMessageHandler on the SOC and ezspIncomingMessageHandler on the host.

Public Attribute Documentation#

type#

EmberIncomingMessageType EmberAfIncomingMessage::type

The type of the incoming message


Definition at line 283 of file ./app/framework/include/af-types.h

apsFrame#

EmberApsFrame* EmberAfIncomingMessage::apsFrame

APS frame for the incoming message


Definition at line 287 of file ./app/framework/include/af-types.h

message#

uint8_t* EmberAfIncomingMessage::message

The message copied into a flat buffer


Definition at line 291 of file ./app/framework/include/af-types.h

msgLen#

uint16_t EmberAfIncomingMessage::msgLen

Length of the incoming message


Definition at line 295 of file ./app/framework/include/af-types.h

source#

uint16_t EmberAfIncomingMessage::source

Two byte node id of the sending node.


Definition at line 299 of file ./app/framework/include/af-types.h

lastHopLqi#

uint8_t EmberAfIncomingMessage::lastHopLqi

Link quality from the node that last relayed the message.


Definition at line 304 of file ./app/framework/include/af-types.h

lastHopRssi#

int8_t EmberAfIncomingMessage::lastHopRssi

The energy level (in units of dBm) observed during the reception.


Definition at line 308 of file ./app/framework/include/af-types.h

bindingTableIndex#

uint8_t EmberAfIncomingMessage::bindingTableIndex

The index of a binding that matches the message or 0xFF if there is no matching binding.


Definition at line 313 of file ./app/framework/include/af-types.h

addressTableIndex#

uint8_t EmberAfIncomingMessage::addressTableIndex

The index of the entry in the address table that matches the sender of the message or 0xFF if there is no matching entry.


Definition at line 319 of file ./app/framework/include/af-types.h

networkIndex#

uint8_t EmberAfIncomingMessage::networkIndex

The index of the network on which this message was received.


Definition at line 323 of file ./app/framework/include/af-types.h