Public Attribute Documentation#

valid#

bool EmberAfPluginPriceClientPrice::valid

Definition at line 973 of file ./app/framework/include/af-types.h

active#

bool EmberAfPluginPriceClientPrice::active

Definition at line 974 of file ./app/framework/include/af-types.h

clientEndpoint#

uint8_t EmberAfPluginPriceClientPrice::clientEndpoint

Definition at line 975 of file ./app/framework/include/af-types.h

providerId#

uint32_t EmberAfPluginPriceClientPrice::providerId

Definition at line 976 of file ./app/framework/include/af-types.h

rateLabel#

uint8_t EmberAfPluginPriceClientPrice::rateLabel[ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH+1]

Definition at line 977 of file ./app/framework/include/af-types.h

issuerEventId#

uint32_t EmberAfPluginPriceClientPrice::issuerEventId

Definition at line 978 of file ./app/framework/include/af-types.h

currentTime#

uint32_t EmberAfPluginPriceClientPrice::currentTime

Definition at line 979 of file ./app/framework/include/af-types.h

unitOfMeasure#

uint8_t EmberAfPluginPriceClientPrice::unitOfMeasure

Definition at line 980 of file ./app/framework/include/af-types.h

currency#

uint16_t EmberAfPluginPriceClientPrice::currency

Definition at line 981 of file ./app/framework/include/af-types.h

priceTrailingDigitAndPriceTier#

uint8_t EmberAfPluginPriceClientPrice::priceTrailingDigitAndPriceTier

Definition at line 982 of file ./app/framework/include/af-types.h

numberOfPriceTiersAndRegisterTier#

uint8_t EmberAfPluginPriceClientPrice::numberOfPriceTiersAndRegisterTier

Definition at line 983 of file ./app/framework/include/af-types.h

startTime#

uint32_t EmberAfPluginPriceClientPrice::startTime

Definition at line 984 of file ./app/framework/include/af-types.h

endTime#

uint32_t EmberAfPluginPriceClientPrice::endTime

Definition at line 985 of file ./app/framework/include/af-types.h

durationInMinutes#

uint16_t EmberAfPluginPriceClientPrice::durationInMinutes

Definition at line 986 of file ./app/framework/include/af-types.h

price#

uint32_t EmberAfPluginPriceClientPrice::price

Definition at line 987 of file ./app/framework/include/af-types.h

priceRatio#

uint8_t EmberAfPluginPriceClientPrice::priceRatio

Definition at line 988 of file ./app/framework/include/af-types.h

generationPrice#

uint32_t EmberAfPluginPriceClientPrice::generationPrice

Definition at line 989 of file ./app/framework/include/af-types.h

generationPriceRatio#

uint8_t EmberAfPluginPriceClientPrice::generationPriceRatio

Definition at line 990 of file ./app/framework/include/af-types.h

alternateCostDelivered#

uint32_t EmberAfPluginPriceClientPrice::alternateCostDelivered

Definition at line 991 of file ./app/framework/include/af-types.h

alternateCostUnit#

uint8_t EmberAfPluginPriceClientPrice::alternateCostUnit

Definition at line 992 of file ./app/framework/include/af-types.h

alternateCostTrailingDigit#

uint8_t EmberAfPluginPriceClientPrice::alternateCostTrailingDigit

Definition at line 993 of file ./app/framework/include/af-types.h

numberOfBlockThresholds#

uint8_t EmberAfPluginPriceClientPrice::numberOfBlockThresholds

Definition at line 994 of file ./app/framework/include/af-types.h

priceControl#

uint8_t EmberAfPluginPriceClientPrice::priceControl

Definition at line 995 of file ./app/framework/include/af-types.h