A data struct for all the trust center backup data.

The 'keyList' pointer must point to an array and 'maxKeyListLength' must be populated with the maximum number of entries the array can hold.

Functions that modify this data structure will populate 'keyListLength' indicating how many keys were actually written into 'keyList'.

Public Attribute Documentation#

extendedPanId#

EmberEUI64 EmberAfTrustCenterBackupData::extendedPanId

Definition at line 1475 of file ./app/framework/include/af-types.h

keyListLength#

uint8_t EmberAfTrustCenterBackupData::keyListLength

Definition at line 1476 of file ./app/framework/include/af-types.h

maxKeyListLength#

uint8_t EmberAfTrustCenterBackupData::maxKeyListLength

Definition at line 1477 of file ./app/framework/include/af-types.h

keyList#

EmberAfLinkKeyBackupData* EmberAfTrustCenterBackupData::keyList

Definition at line 1478 of file ./app/framework/include/af-types.h