A data struct for the information retrieved during a response to an Ember Bootloader over-the-air query.

Public Attributes#

uint8_t
uint16_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

hardwareTag#

uint8_t EmberAfStandaloneBootloaderQueryResponseData::hardwareTag[EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH]

eui64#

uint8_t EmberAfStandaloneBootloaderQueryResponseData::eui64[EUI64_SIZE]

mfgId#

uint16_t EmberAfStandaloneBootloaderQueryResponseData::mfgId

bootloaderVersion#

uint16_t EmberAfStandaloneBootloaderQueryResponseData::bootloaderVersion

capabilities#

uint8_t EmberAfStandaloneBootloaderQueryResponseData::capabilities

platform#

uint8_t EmberAfStandaloneBootloaderQueryResponseData::platform

micro#

uint8_t EmberAfStandaloneBootloaderQueryResponseData::micro

phy#

uint8_t EmberAfStandaloneBootloaderQueryResponseData::phy

bootloaderActive#

bool EmberAfStandaloneBootloaderQueryResponseData::bootloaderActive