A structure used to store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.

Public Attributes#

uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

endpoint#

uint8_t EmberAfSceneTableEntry::endpoint

Definition at line 897 of file ./app/framework/include/af-types.h

groupId#

uint16_t EmberAfSceneTableEntry::groupId

Definition at line 898 of file ./app/framework/include/af-types.h

sceneId#

uint8_t EmberAfSceneTableEntry::sceneId

Definition at line 899 of file ./app/framework/include/af-types.h

transitionTime#

uint16_t EmberAfSceneTableEntry::transitionTime

Definition at line 903 of file ./app/framework/include/af-types.h

transitionTime100ms#

uint8_t EmberAfSceneTableEntry::transitionTime100ms

Definition at line 904 of file ./app/framework/include/af-types.h