Use for default values.
Default value is either a value itself, if it is 2 bytes or less, or a pointer to the value itself, if attribute type is longer than 2 bytes.
Public Attribute Documentation#
ptrToDefaultValue#
uint8_t* EmberAfDefaultAttributeValue::ptrToDefaultValue
Point to data if size is more than 2 bytes. If size is more than 2 bytes and this value is NULL, the default value is all zeroes.
Definition at line
118
of file app/framework/include/af-types.h
defaultValue#
uint16_t EmberAfDefaultAttributeValue::defaultValue
Actual default value if the attribute size is 2 bytes or less.
Definition at line
122
of file app/framework/include/af-types.h