Contain endpoint information about a device.

Public Attribute Documentation#

eui64#

EmberEUI64 EmberAfDeviceInfo::eui64

Definition at line 1951 of file app/framework/include/af-types.h

endpoints#

EmberAfEndpointInfoStruct EmberAfDeviceInfo::endpoints[EMBER_AF_MAX_ENDPOINTS_PER_DEVICE]

Definition at line 1952 of file app/framework/include/af-types.h

status#

EmberAfDeviceDiscoveryStatus EmberAfDeviceInfo::status

Definition at line 1953 of file app/framework/include/af-types.h

discoveryFailures#

uint8_t EmberAfDeviceInfo::discoveryFailures

Definition at line 1954 of file app/framework/include/af-types.h

capabilities#

uint8_t EmberAfDeviceInfo::capabilities

Definition at line 1955 of file app/framework/include/af-types.h

endpointCount#

uint8_t EmberAfDeviceInfo::endpointCount

Definition at line 1956 of file app/framework/include/af-types.h

stackRevision#

uint8_t EmberAfDeviceInfo::stackRevision

Definition at line 1957 of file app/framework/include/af-types.h