Store group table entries in RAM or in tokens, depending on the platform. If the endpoint field is EMBER_AF_GROUP_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

endpoint#

uint8_t EmberAfGroupTableEntry::endpoint

Definition at line 920 of file app/framework/include/af-types.h

groupId#

uint16_t EmberAfGroupTableEntry::groupId

Definition at line 921 of file app/framework/include/af-types.h

bindingIndex#

uint8_t EmberAfGroupTableEntry::bindingIndex

Definition at line 922 of file app/framework/include/af-types.h