You are viewing documentation for version:
Describe a load control event.
This struct is used in the load control event callback and within the demand response load control cluster code.
Public Attribute Documentation#
eventId#
uint32_t EmberAfLoadControlEvent::eventId
destinationEndpoint#
uint8_t EmberAfLoadControlEvent::destinationEndpoint
deviceClass#
uint16_t EmberAfLoadControlEvent::deviceClass
utilityEnrollmentGroup#
uint8_t EmberAfLoadControlEvent::utilityEnrollmentGroup
startTime#
uint32_t EmberAfLoadControlEvent::startTime
Start time in seconds
duration#
uint16_t EmberAfLoadControlEvent::duration
Duration in minutes
criticalityLevel#
uint8_t EmberAfLoadControlEvent::criticalityLevel
coolingTempOffset#
uint8_t EmberAfLoadControlEvent::coolingTempOffset
heatingTempOffset#
uint8_t EmberAfLoadControlEvent::heatingTempOffset
coolingTempSetPoint#
int16_t EmberAfLoadControlEvent::coolingTempSetPoint
heatingTempSetPoint#
int16_t EmberAfLoadControlEvent::heatingTempSetPoint
avgLoadPercentage#
int8_t EmberAfLoadControlEvent::avgLoadPercentage
dutyCycle#
uint8_t EmberAfLoadControlEvent::dutyCycle
eventControl#
uint8_t EmberAfLoadControlEvent::eventControl
startRand#
uint32_t EmberAfLoadControlEvent::startRand
durationRand#
uint32_t EmberAfLoadControlEvent::durationRand
optionControl#
uint8_t EmberAfLoadControlEvent::optionControl