This structure is an in-memory representation of the Over-the-air header data that resides on disk. It is not a byte-for-byte copy.
Public Attributes#
The spec. does not require that the string be NULL terminated in the header stored on disk. Therefore, +1 is added in the data structure to ensure support of 32-character string without a NULL terminator.
When reading the header, this will be the complete length of the file. When writing the header, this must be set to the length of the MFG image data portion including all tags.
The remaining four fields are optional. Check the field control to determine if their values are valid.
Public Attribute Documentation#
headerVersion#
uint16_t EmberAfOtaHeader::headerVersion
1309
of file app/framework/include/af-types.h
headerLength#
uint16_t EmberAfOtaHeader::headerLength
1310
of file app/framework/include/af-types.h
fieldControl#
uint16_t EmberAfOtaHeader::fieldControl
1311
of file app/framework/include/af-types.h
manufacturerId#
uint16_t EmberAfOtaHeader::manufacturerId
1312
of file app/framework/include/af-types.h
imageTypeId#
uint16_t EmberAfOtaHeader::imageTypeId
1313
of file app/framework/include/af-types.h
firmwareVersion#
uint32_t EmberAfOtaHeader::firmwareVersion
1314
of file app/framework/include/af-types.h
zigbeeStackVersion#
uint16_t EmberAfOtaHeader::zigbeeStackVersion
1315
of file app/framework/include/af-types.h
headerString#
uint8_t EmberAfOtaHeader::headerString[EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH+1]
The spec. does not require that the string be NULL terminated in the header stored on disk. Therefore, +1 is added in the data structure to ensure support of 32-character string without a NULL terminator.
1322
of file app/framework/include/af-types.h
imageSize#
uint32_t EmberAfOtaHeader::imageSize
When reading the header, this will be the complete length of the file. When writing the header, this must be set to the length of the MFG image data portion including all tags.
1329
of file app/framework/include/af-types.h
securityCredentials#
uint8_t EmberAfOtaHeader::securityCredentials
The remaining four fields are optional. Check the field control to determine if their values are valid.
1335
of file app/framework/include/af-types.h
EUI64#
uint8_t EmberAfOtaHeader::EUI64[EUI64_SIZE]
1337
of file app/framework/include/af-types.h
UID#
uint8_t EmberAfOtaHeader::UID[UID_SIZE]
1338
of file app/framework/include/af-types.h
upgradeFileDestination#
union EmberAfOtaHeader::@3 EmberAfOtaHeader::upgradeFileDestination
1339
of file app/framework/include/af-types.h
minimumHardwareVersion#
uint16_t EmberAfOtaHeader::minimumHardwareVersion
1340
of file app/framework/include/af-types.h
maximumHardwareVersion#
uint16_t EmberAfOtaHeader::maximumHardwareVersion
1341
of file app/framework/include/af-types.h