Interpan header used for sending and receiving interpan messages.
Public Attribute Documentation#
messageType#
EmberAfInterpanMessageType EmberAfInterpanHeader::messageType
Definition at line
371
of file app/framework/include/af-types.h
longAddress#
EmberEUI64 EmberAfInterpanHeader::longAddress
MAC addressing, which is the destination for outgoing messages and source for incoming messages, which always has a long address.
Definition at line
378
of file app/framework/include/af-types.h
shortAddress#
EmberNodeId EmberAfInterpanHeader::shortAddress
Definition at line
379
of file app/framework/include/af-types.h
panId#
EmberPanId EmberAfInterpanHeader::panId
Definition at line
380
of file app/framework/include/af-types.h
profileId#
EmberAfProfileId EmberAfInterpanHeader::profileId
APS data
Definition at line
385
of file app/framework/include/af-types.h
clusterId#
EmberAfClusterId EmberAfInterpanHeader::clusterId
Definition at line
386
of file app/framework/include/af-types.h
groupId#
EmberMulticastId EmberAfInterpanHeader::groupId
The groupId is only used for EMBER_AF_INTERPAN_MULTICAST
Definition at line
391
of file app/framework/include/af-types.h
options#
EmberAfInterpanOptions EmberAfInterpanHeader::options
Definition at line
392
of file app/framework/include/af-types.h