General#

General commands that are applicable to the node regardless of clusters or plugins.

Macros#

#define

zcl mfg-code [mfgSpecificId:2]

#define

zcl time [utcTime:4]

#define

zcl use-next-sequence [useNextSequence:1]

#define

zcl x-default-resp [disableDefaultResponse:1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_MFG_CODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_MFG_CODE

zcl mfg-code [mfgSpecificId:2]

  • Sets the two byte manufacturer specific identifier to use for the next command if the command is not already built.

    • mfgSpecificId - INT16U - Manufacturer Specific Id


Definition at line 31 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_TIME#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_TIME

zcl time [utcTime:4]

  • Cli command to call emberAfSetTime function documented in af.h

    • utcTime - INT32U - ZigBee UTC time, number of seconds since the year 2000


Definition at line 37 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_USE_NEXT_SEQUENCE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_USE_NEXT_SEQUENCE

zcl use-next-sequence [useNextSequence:1]

  • Sets the flag to use the incremented sequence number from the framework for the next raw command.

    • useNextSequence - BOOLEAN - bool value indicating whether raw command will use the incremented seq number from framework, set(1) or not(0).


Definition at line 43 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_X_DEFAULT_RESP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_X_DEFAULT_RESP

zcl x-default-resp [disableDefaultResponse:1]

  • Sets the Disable Default Response Frame Control bit to use for the next command if the command is not already built.

    • disableDefaultResponse - BOOLEAN - bool value indicating whether the disable default response bit is set(1) or not (0).


Definition at line 49 of file app/framework/test/headers/cli.doc