Cluster Commands: IAS Zone#

This group describes the CLI commands for the IAS Zone cluster. Listed below is a description of the cluster: Attributes and commands for IAS security zone devices.

Macros#

#define

zcl ias-zone sc [zoneStatus:2] [extendedStatus:1] [zoneId:1] [delay:2]

#define

zcl ias-zone enroll [zoneType:2] [manufacturerCode:2]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_SC#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_SC

zcl ias-zone sc [zoneStatus:2] [extendedStatus:1] [zoneId:1] [delay:2]

  • Command description for zoneStatusChangeNotification

    • zoneStatus - IasZoneStatus [BITMAP16]

    • extendedStatus - BITMAP8

    • zoneId - INT8U

    • delay - INT16U


Definition at line 1220 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_ENROLL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_ENROLL

zcl ias-zone enroll [zoneType:2] [manufacturerCode:2]

  • Command description for zoneEnrollRequest


Definition at line 1229 of file app/framework/test/headers/cli.doc