Standalone Bootloader Server#
API and Callbacks for the Standalone Bootloader Server Component.
This component implements the legacy Ember over-the-air, 1-hop, bootload protocol. This can bootload a target node that has a standalone bootloader client running on it. It first scans for neighboring devices supporting the protocol. Once a client target has been identified, it sends the request to bootload, answers the challenge using the configured encryption key, and then transfers a new EBL file via Xmodem using 802.15.4 MAC data frames. It utilizes the OTA Storage code to retrieve the EBL file for sending to the target node. This is not a Zigbee-certifiable protocol.
Modules#
API#
EmberStatus
EmberStatus
emberAfPluginStandaloneBootloaderServerStartClientBootload(EmberEUI64 longId, const EmberAfOtaImageId *id, uint16_t tag)
EmberStatus
emberAfPluginStandaloneBootloaderServerStartClientBootloadWithCurrentTarget(const EmberAfOtaImageId *id, uint16_t tag)
API Documentation#
emberAfPluginStandaloneBootloaderServerBroadcastQuery#
EmberStatus emberAfPluginStandaloneBootloaderServerBroadcastQuery (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emberAfPluginStandaloneBootloaderServerStartClientBootload#
EmberStatus emberAfPluginStandaloneBootloaderServerStartClientBootload (EmberEUI64 longId, const EmberAfOtaImageId * id, uint16_t tag)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | longId | |
| const EmberAfOtaImageId * | N/A | id | |
| uint16_t | N/A | tag |
emberAfPluginStandaloneBootloaderServerStartClientBootloadWithCurrentTarget#
EmberStatus emberAfPluginStandaloneBootloaderServerStartClientBootloadWithCurrentTarget (const EmberAfOtaImageId * id, uint16_t tag)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberAfOtaImageId * | N/A | id | |
| uint16_t | N/A | tag |