ZLL Level Control Server#
API and Callbacks for the ZLL Level Control Cluster Server Component.
Silicon Labs implementation of the original Zigbee Light Link profile enhancements to the Level Control server cluster. The component is only intended to assist with debugging, as the implemented callbacks simply parse requests from the Identify client and blink LEDs. Before production, this component should be replaced with code that acts on the requests in an appropriate way. Note that the extensions do not now require Touchlink commissioning to be used, and that the commands may now be required by other device types, such as Lighting and Occupancy.
API#
emberAfPluginZllLevelControlServerMoveToLevelWithOnOffZllExtensions(const EmberAfClusterCommand *cmd)
bool
emberAfPluginZllLevelControlServerIgnoreMoveToLevelMoveStepStop(uint8_t endpoint, uint8_t commandId)
Macros#
#define
EMBER_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MINIMUM_LEVEL 0x01
#define
EMBER_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MAXIMUM_LEVEL 0xFE
API Documentation#
emberAfPluginZllLevelControlServerMoveToLevelWithOnOffZllExtensions#
EmberAfStatus emberAfPluginZllLevelControlServerMoveToLevelWithOnOffZllExtensions (const EmberAfClusterCommand * cmd)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberAfClusterCommand * | N/A | cmd |
emberAfPluginZllLevelControlServerIgnoreMoveToLevelMoveStepStop#
bool emberAfPluginZllLevelControlServerIgnoreMoveToLevelMoveStepStop (uint8_t endpoint, uint8_t commandId)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | |
| uint8_t | N/A | commandId |