Cluster Commands: BACnet Protocol Tunnel#
This group describes the CLI commands for the BACnet Protocol Tunnel cluster. Listed below is a description of the cluster:
Commands and attributes required to tunnel the BACnet protocol.
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS
zcl bacnet transfer-npdu whois
Send a sample whois command.
EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM
zcl bacnet transfer-npdu random [npdu:1]
This command is generated when a BACnet network layer wishes to transfer a BACnet NPDU across a ZigBee tunnel to another BACnet network layer.
npdu - DATA8