Cluster Commands: Prepayment#
This group describes the CLI commands for the Prepayment cluster. Listed below is a description of the cluster:
The Prepayment Cluster provides the facility to pass messages relating to prepayment between devices on the HAN.
Macros#
zcl prepayment sel-av-em-cred [commandIssueDateTime:4] [originatingDevice:1] [siteId:-1] [meterSerialNumber:-1]
zcl prepayment chg-debt [issuerEventId:4] [debtLabel:-1] [debtAmount:4] [debtRecoveryMethod:1] [debtAmountType:1] [debtRecoveryStartTime:4] [debtRecoveryCollectionTime:2] [debtRecoveryFrequency:1] [debtRecoveryAmount:4] [debtRecoveryBalancePercentage:2]
zcl prepayment em-cred-setup [issuerEventId:4] [startTime:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4]
zcl prepayment cons-top-up [originatingDevice:1] [topUpCode:-1]
zcl prepayment cred-adj [issuerEventId:4] [startTime:4] [creditAdjustmentType:1] [creditAdjustmentValue:4]
zcl prepayment chg-pmt-mode [providerId:4] [issuerEventId:4] [implementationDateTime:4] [proposedPaymentControlConfiguration:2] [cutOffValue:4]
zcl prepayment get-pp-ss [earliestStartTime:4] [latestEndTime:4] [snapshotOffset:1] [snapshotCause:4]
zcl prepayment get-top-up-log [latestEndTime:4] [numberOfRecords:1]
zcl prepayment set-low-cred-wng-lvl [lowCreditWarningLevel:4]
zcl prepayment get-debt-repmt-log [latestEndTime:4] [numberOfDebts:1] [debtType:1]
zcl prepayment set-max-cred-lmt [providerId:4] [issuerEventId:4] [implementationDateTime:4] [maximumCreditLevel:4] [maximumCreditPerTopUp:4]
zcl prepayment set-oa-debt-cap [providerId:4] [issuerEventId:4] [implementationDateTime:4] [overallDebtCap:4]
zcl prepayment pub-prep-ss [snapshotId:4] [snapshotTime:4] [totalSnapshotsFound:1] [commandIndex:1] [totalNumberOfCommands:1] [snapshotCause:4] [snapshotPayloadType:1] [snapshotPayload:1]
zcl prepayment chg-pmt-mode-resp [friendlyCredit:1] [friendlyCreditCalendarId:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4]
zcl prepayment cons-top-up-resp [resultType:1] [topUpValue:4] [sourceOfTopUp:1] [creditRemaining:4]
zcl prepayment pub-top-up-log [commandIndex:1] [totalNumberOfCommands:1] [topUpPayload:7]
zcl prepayment pub-debt-log [commandIndex:1] [totalNumberOfCommands:1] [debtPayload:13]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SEL_AV_EM_CRED#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SEL_AV_EM_CRED
zcl prepayment sel-av-em-cred [commandIssueDateTime:4] [originatingDevice:1] [siteId:-1] [meterSerialNumber:-1]
This command is sent to the Metering Device to activate the use of any Emergency Credit available on the Metering Device.
commandIssueDateTime - UTC_TIME
originatingDevice - OriginatingDevice [ENUM8]
siteId - OCTET_STRING
meterSerialNumber - OCTET_STRING See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_DEBT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_DEBT
zcl prepayment chg-debt [issuerEventId:4] [debtLabel:-1] [debtAmount:4] [debtRecoveryMethod:1] [debtAmountType:1] [debtRecoveryStartTime:4] [debtRecoveryCollectionTime:2] [debtRecoveryFrequency:1] [debtRecoveryAmount:4] [debtRecoveryBalancePercentage:2]
The ChangeDebt command is send to the Metering Device to change the fuel or Non fuel debt values.
issuerEventId - INT32U
debtLabel - OCTET_STRING
debtAmount - INT32U
debtRecoveryMethod - DebtRecoveryMethod [ENUM8]
debtAmountType - DebtAmountType [ENUM8]
debtRecoveryStartTime - UTC_TIME
debtRecoveryCollectionTime - INT16U
debtRecoveryFrequency - DebtRecoveryFrequency [ENUM8]
debtRecoveryAmount - INT32U
debtRecoveryBalancePercentage - INT16U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_EM_CRED_SETUP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_EM_CRED_SETUP
zcl prepayment em-cred-setup [issuerEventId:4] [startTime:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4]
This command is a method to set up the parameters for the emergency credit.
issuerEventId - INT32U
startTime - UTC_TIME
emergencyCreditLimit - INT32U
emergencyCreditThreshold - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP
zcl prepayment cons-top-up [originatingDevice:1] [topUpCode:-1]
The ConsumerTopUp command is used by the IPD and the ESI as a method of applying credit top up values to the prepayment meter.
originatingDevice - OriginatingDevice [ENUM8]
topUpCode - OCTET_STRING See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CRED_ADJ#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CRED_ADJ
zcl prepayment cred-adj [issuerEventId:4] [startTime:4] [creditAdjustmentType:1] [creditAdjustmentValue:4]
The CreditAdjustment command is sent to update the accounting base for the Prepayment meter.
issuerEventId - INT32U
startTime - UTC_TIME
creditAdjustmentType - CreditAdjustmentType [ENUM8]
creditAdjustmentValue - INT32U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE
zcl prepayment chg-pmt-mode [providerId:4] [issuerEventId:4] [implementationDateTime:4] [proposedPaymentControlConfiguration:2] [cutOffValue:4]
This command is sent to a Metering Device to instruct it to change its mode of operation. i.e. from Credit to Prepayment.
providerId - INT32U
issuerEventId - INT32U
implementationDateTime - UTC_TIME
proposedPaymentControlConfiguration - sli_zigbee_payment_control_configuration_t [BITMAP16]
cutOffValue - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_PP_SS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_PP_SS
zcl prepayment get-pp-ss [earliestStartTime:4] [latestEndTime:4] [snapshotOffset:1] [snapshotCause:4]
This command is used to request the cluster server for snapshot data.
earliestStartTime - UTC_TIME
latestEndTime - UTC_TIME
snapshotOffset - INT8U
snapshotCause - sli_zigbee_prepay_snapshot_payload_cause_t [BITMAP32]
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_TOP_UP_LOG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_TOP_UP_LOG
zcl prepayment get-top-up-log [latestEndTime:4] [numberOfRecords:1]
This command is sent to the Metering Device to retrieve the log of Top Up codes received by the meter.
latestEndTime - UTC_TIME
numberOfRecords - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_LOW_CRED_WNG_LVL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_LOW_CRED_WNG_LVL
zcl prepayment set-low-cred-wng-lvl [lowCreditWarningLevel:4]
This command is sent from client to a Prepayment server to set the warning level for low credit.
lowCreditWarningLevel - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_DEBT_REPMT_LOG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_DEBT_REPMT_LOG
zcl prepayment get-debt-repmt-log [latestEndTime:4] [numberOfDebts:1] [debtType:1]
This command is used to request the contents of the repayment log.
latestEndTime - UTC_TIME
numberOfDebts - INT8U
debtType - RepaymentDebtType [ENUM8] See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_MAX_CRED_LMT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_MAX_CRED_LMT
zcl prepayment set-max-cred-lmt [providerId:4] [issuerEventId:4] [implementationDateTime:4] [maximumCreditLevel:4] [maximumCreditPerTopUp:4]
This command is sent from a client to the Prepayment server to set the maximum credit level allowed in the meter.
providerId - INT32U
issuerEventId - INT32U
implementationDateTime - UTC_TIME
maximumCreditLevel - INT32U
maximumCreditPerTopUp - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_OA_DEBT_CAP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_OA_DEBT_CAP
zcl prepayment set-oa-debt-cap [providerId:4] [issuerEventId:4] [implementationDateTime:4] [overallDebtCap:4]
This command is sent from a client to the Prepayment server to set the overall debt cap allowed in the meter.
providerId - INT32U
issuerEventId - INT32U
implementationDateTime - UTC_TIME
overallDebtCap - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_PREP_SS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_PREP_SS
zcl prepayment pub-prep-ss [snapshotId:4] [snapshotTime:4] [totalSnapshotsFound:1] [commandIndex:1] [totalNumberOfCommands:1] [snapshotCause:4] [snapshotPayloadType:1] [snapshotPayload:1]
This command is generated in response to a GetPrepaySnapshot command. It is used to return a single snapshot to the client.
snapshotId - INT32U
snapshotTime - UTC_TIME
totalSnapshotsFound - INT8U
commandIndex - INT8U
totalNumberOfCommands - INT8U
snapshotCause - sli_zigbee_prepay_snapshot_payload_cause_t [BITMAP32]
snapshotPayloadType - sli_zigbee_prepay_snapshot_payload_type_t [ENUM8]
snapshotPayload - INT8U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE_RESP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE_RESP
zcl prepayment chg-pmt-mode-resp [friendlyCredit:1] [friendlyCreditCalendarId:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4]
This command is send in response to the ChangePaymentMode Command.
friendlyCredit - sli_zigbee_friendly_credit_t [BITMAP8]
friendlyCreditCalendarId - INT32U
emergencyCreditLimit - INT32U
emergencyCreditThreshold - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP_RESP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP_RESP
zcl prepayment cons-top-up-resp [resultType:1] [topUpValue:4] [sourceOfTopUp:1] [creditRemaining:4]
This command is send in response to the ConsumerTopUp Command.
resultType - ResultType [ENUM8]
topUpValue - INT32U
sourceOfTopUp - OriginatingDevice [ENUM8]
creditRemaining - INT32U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_TOP_UP_LOG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_TOP_UP_LOG
zcl prepayment pub-top-up-log [commandIndex:1] [totalNumberOfCommands:1] [topUpPayload:7]
This command is used to send the Top Up Code Log entries to the client.
commandIndex - INT8U
totalNumberOfCommands - INT8U
topUpPayload - struct sl_zigbee_zcl_top_up_payload_t
EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_DEBT_LOG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_DEBT_LOG
zcl prepayment pub-debt-log [commandIndex:1] [totalNumberOfCommands:1] [debtPayload:13]
This command is used to send the contents of the Repayment Log.
commandIndex - INT8U
totalNumberOfCommands - INT8U
debtPayload - struct sl_zigbee_zcl_debt_payload_t