Green Power Server#

API and Callbacks for the Green Power Cluster Server Component.

A component implementing the server-side functionality of the Green Power cluster.

Modules#

sl_zigbee_af_green_power_server_commissioning_state_t

sli_zigbee_gp_device_id_and_command_map_t

sli_zigbee_gp_device_id_and_cluster_map_t

sli_zigbee_zigbee_cluster_t

sli_zigbee_gp_comm_data_saved_t

Green Power Server

API#

Get a GPD commissioning instance in a multiple GPD commissioning session.

void

Delete a GPD commissioning instance in a multiple GPD commissioning session.

void

Extend the commissioning window of a commissioning session.

sl_zigbee_af_green_power_server_derive_shared_key_from_sink_attribute(uint8_t *gpsSecurityKeyTypeAtrribute, sl_zigbee_key_data_t *gpSharedKeyAttribute, sl_zigbee_gp_address_t *gpdAddr)

Derive the shared key from the sink attributes.

void
sl_zigbee_af_green_power_server_remove_sink_entry(sl_zigbee_gp_address_t *gpdAddr)

Clears the entry for a GPD in sink table.

bool

Close the commissioning window of current commissioning session.

Enumerations#

enum
GREEN_POWER_SERVER_GPS_NODE_STATE_NOT_IN_NETWORK
GREEN_POWER_SERVER_GPS_NODE_STATE_IN_NETWORK
}
enum
GREEN_POWER_SERVER_SINK_TABLE_ACCESS_TYPE_REMOVE_GPD
GREEN_POWER_SERVER_SINK_TABLE_ACCESS_TYPE_ADD_GPD
GREEN_POWER_SERVER_SINK_TABLE_ACCESS_TYPE_UNKNOWN
}
enum
GP_SINK_COMM_STATE_IDLE
GP_SINK_COMM_STATE_COLLECT_REPORTS
GP_SINK_COMM_STATE_SEND_COMM_REPLY
GP_SINK_COMM_STATE_WAIT_FOR_SUCCESS
GP_SINK_COMM_STATE_FINALISE_PAIRING
GP_SINK_COMM_STATE_PAIRING_DONE
}
enum
COMMISSIONING_TIMEOUT_TYPE_GENERIC_SWITCH = 0
COMMISSIONING_TIMEOUT_TYPE_MULTI_SENSOR = 1
COMMISSIONING_TIMEOUT_TYPE_COMMISSIONING_WINDOW_TIMEOUT = 2
}
enum
SINK_PAIRING_STATUS_SUCCESS = 0
SINK_PAIRING_STATUS_FAILURE = 1
SINK_PAIRING_STATUS_IN_PROGRESS = 2
SINK_PAIRING_STATUS_FAIL_NO_MATCHING_FUNCTIONALITY = 3
SINK_PAIRING_STATUS_FAIL_ADDING_TRANSLATION = 4
SINK_PAIRING_STATUS_FAIL_NO_SPACE_IN_SINK_TABLE = 5
SINK_PAIRING_STATUS_FAIL_ENTRY_CORRUPTED = 6
}
enum
GP_PRE_SINK_PAIRING_CALLBACK_SOURCE_UNKNOWN = 0
GP_PRE_SINK_PAIRING_CALLBACK_COMMISSONING_FINALIZE = 1
GP_PRE_SINK_PAIRING_CALLBACK_PAIRING_CONFIGURATION = 2
}

Typedefs#

typedef uint8_t

GP Server network state.

typedef uint8_t

Describes how the GP server accesses or updates the sink table.

typedef uint8_t

Represents the current state of GP sink commissioning.

typedef uint8_t

Specifies the type of timeout used during GP sink commissioning.

typedef uint8_t

Indicates the result or status of a GP sink pairing attempt.

typedef uint8_t

Identifies the source that triggered the pre-sink-pairing callback.

Cached commissioning information for a Green Power Device (GPD).

Macros#

#define
#define
GP_DEFAULT_LINK_KEY { 0x5A, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6C, 0x6C, 0x69, 0x61, 0x6E, 0x63, 0x65, 0x30, 0x39 }
#define
genericSwitchCommissioningTimeout (&sl_zigbee_af_green_power_server_generic_switch_commissioning_timeout_event)
#define
multiSensorCommissioningTimeout (&sl_zigbee_af_green_power_server_multi_sensor_commissioning_timeout_event)
#define
commissioningWindowTimeout (&sl_zigbee_af_green_power_server_commissioning_window_timeout_event)

API Documentation#

sl_zigbee_af_green_power_server_find_commissioning_gpd_instance#

sl_zigbee_commissioning_gpd_t * sl_zigbee_af_green_power_server_find_commissioning_gpd_instance (sl_zigbee_gp_address_t * gpdAddr)

Get a GPD commissioning instance in a multiple GPD commissioning session.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_gp_address_t *[in]gpdAddr

GPD address

The green power server can be configured to allow multiple GPDs to commission within a commissioning session. Given a GPD instance address, this function will find the currently-commissioning GPD instance. This is a helpful indicator of the commissioning progress of a given GPD when multi GPDS are commissioning in a commissioning window.

Returns


sl_zigbee_af_green_power_server_delete_commissioning_gpd_instance#

void sl_zigbee_af_green_power_server_delete_commissioning_gpd_instance (sl_zigbee_gp_address_t * gpdAddr)

Delete a GPD commissioning instance in a multiple GPD commissioning session.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_gp_address_t *[in]gpdAddr

GPD address

The green power server can be configured to allow multiple GPDs to commission within a commissioning session. Given a GPD instance address, this function will find and delete the currently-commissioning GPD instance. This is a helpful way to remove unwanted GPD instances in a multiple GPD commissioning session.


sl_zigbee_af_green_power_cluster_gp_sink_commissioning_window_extend#

void sl_zigbee_af_green_power_cluster_gp_sink_commissioning_window_extend (uint16_t commissioningWindow)

Extend the commissioning window of a commissioning session.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]commissioningWindow

Commissioning window to be extended from this point in time in seconds

This is a helper function that sends out a proxy commissioning mode from the server side to all proxies in the network. It internally uses the same parameters used previously in the proxy commissioning mode with action = enter.


sl_zigbee_af_green_power_cluster_get_server_commissioning_sate#

sl_zigbee_af_green_power_server_commissioning_state_t * sl_zigbee_af_green_power_cluster_get_server_commissioning_sate (void )

Get the commissioning state of the green power server.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function gets the commissioning state of the green power server.

Returns


sl_zigbee_af_green_power_server_derive_shared_key_from_sink_attribute#

sl_zigbee_af_status_t sl_zigbee_af_green_power_server_derive_shared_key_from_sink_attribute (uint8_t * gpsSecurityKeyTypeAtrribute, sl_zigbee_key_data_t * gpSharedKeyAttribute, sl_zigbee_gp_address_t * gpdAddr)

Derive the shared key from the sink attributes.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[in]gpsSecurityKeyTypeAtrribute

Security key type attribute

sl_zigbee_key_data_t *[out]gpSharedKeyAttribute

Security key attribute

sl_zigbee_gp_address_t *[in]gpdAddr

GPD address

This function derives the shared key used in green power server side using the respective security attribute values.

Returns

  • Status of the key derivation


sl_zigbee_af_green_power_server_remove_sink_entry#

void sl_zigbee_af_green_power_server_remove_sink_entry (sl_zigbee_gp_address_t * gpdAddr)

Clears the entry for a GPD in sink table.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_gp_address_t *[in]gpdAddr

GPD address

This function clears the entries in the sink table for a given gpd. In a sink table, there is unique entry for each GPD based on its addressing. When the GPD addressing uses application id=0b000 with 32 bit sourceId, there is just one entry for each GPD. But, when the GPD addressing with application Id=0b010 that is EUI64 with endpoint id, for each unique endpoint, there can be an entry in sink table. Hence, when this function is called with application Id=0b010,EUI64 with endpoint id=0xff(all endpoints), it clears all the entry for that GPD with supplied EUI64. With clear up the gpd from sink table it also clears the translation table for that GPD.


sl_zigbee_af_green_power_cluster_gp_sink_close_commissioning_window#

bool sl_zigbee_af_green_power_cluster_gp_sink_close_commissioning_window (void )

Close the commissioning window of current commissioning session.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This is a helper function that closes a commissioning session if there is no active GPD commissioning in progress. If the commissioning session started with "InvolveProxy" option, then it also sends out a proxy commissioning mode message with action to exit commissioning from the server side to all proxies in the network. It internally uses the same parameters used previously in the proxy commissioning mode entered but with action as "exit".

Returns

  • Status of the command as true when success or there is no open commissioning window. Returns false for failure of the command for any reason or there is any GPD that is still undergoing commissioning process or a failure.


Enumeration Documentation#

GreenPowerServerGPSNodeState#

GreenPowerServerGPSNodeState
Enumerator
GREEN_POWER_SERVER_GPS_NODE_STATE_NOT_IN_NETWORK

Node not in network

GREEN_POWER_SERVER_GPS_NODE_STATE_IN_NETWORK

Node in network


GreenPowerServerSinkTableAccessType#

GreenPowerServerSinkTableAccessType
Enumerator
GREEN_POWER_SERVER_SINK_TABLE_ACCESS_TYPE_REMOVE_GPD

Remove GPD from Sink Table

GREEN_POWER_SERVER_SINK_TABLE_ACCESS_TYPE_ADD_GPD

Add GPD in Sink Table

GREEN_POWER_SERVER_SINK_TABLE_ACCESS_TYPE_UNKNOWN

Access type unknown


GPSinkCommState#

GPSinkCommState
Enumerator
GP_SINK_COMM_STATE_IDLE

Idle

GP_SINK_COMM_STATE_COLLECT_REPORTS

Collect reports

GP_SINK_COMM_STATE_SEND_COMM_REPLY

Send commissioning reply

GP_SINK_COMM_STATE_WAIT_FOR_SUCCESS

Wait for success

GP_SINK_COMM_STATE_FINALISE_PAIRING

Finalize pairing

GP_SINK_COMM_STATE_PAIRING_DONE

Pairing done


CommissioningTimeoutType#

CommissioningTimeoutType
Enumerator
COMMISSIONING_TIMEOUT_TYPE_GENERIC_SWITCH

Generic switch

COMMISSIONING_TIMEOUT_TYPE_MULTI_SENSOR

Multi-sensor

COMMISSIONING_TIMEOUT_TYPE_COMMISSIONING_WINDOW_TIMEOUT

Commissioning window timeout


PairingStatus#

PairingStatus
Enumerator
SINK_PAIRING_STATUS_SUCCESS

Success

SINK_PAIRING_STATUS_FAILURE

Failure

SINK_PAIRING_STATUS_IN_PROGRESS

In progress

SINK_PAIRING_STATUS_FAIL_NO_MATCHING_FUNCTIONALITY

Failure (No matching functionality)

SINK_PAIRING_STATUS_FAIL_ADDING_TRANSLATION

Failure (Adding translation)

SINK_PAIRING_STATUS_FAIL_NO_SPACE_IN_SINK_TABLE

Failure (No space in sink table)

SINK_PAIRING_STATUS_FAIL_ENTRY_CORRUPTED

Failure (Entry corrupted)


PreSinkPairingCallbackSource#

PreSinkPairingCallbackSource
Enumerator
GP_PRE_SINK_PAIRING_CALLBACK_SOURCE_UNKNOWN

Unknown

GP_PRE_SINK_PAIRING_CALLBACK_COMMISSONING_FINALIZE

Commissioning finalize

GP_PRE_SINK_PAIRING_CALLBACK_PAIRING_CONFIGURATION

Pairing configuration


Typedef Documentation#

sli_zigbee_gps_network_state_t#

typedef uint8_t sli_zigbee_gps_network_state_t

GP Server network state.


sl_zigbee_af_gp_server_sink_table_access_type_t#

typedef uint8_t sl_zigbee_af_gp_server_sink_table_access_type_t

Describes how the GP server accesses or updates the sink table.


sl_zigbee_sink_commission_state_t#

typedef uint8_t sl_zigbee_sink_commission_state_t

Represents the current state of GP sink commissioning.


sl_zigbee_sink_commissioning_timeout_type_t#

typedef uint8_t sl_zigbee_sink_commissioning_timeout_type_t

Specifies the type of timeout used during GP sink commissioning.


sl_zigbee_sink_pairing_status_t#

typedef uint8_t sl_zigbee_sink_pairing_status_t

Indicates the result or status of a GP sink pairing attempt.


sl_zigbee_pre_sink_pairing_callback_source_t#

typedef uint8_t sl_zigbee_pre_sink_pairing_callback_source_t

Identifies the source that triggered the pre-sink-pairing callback.


sl_zigbee_commissioning_gpd_t#

typedef sli_zigbee_gp_comm_data_saved_t sl_zigbee_commissioning_gpd_t

Cached commissioning information for a Green Power Device (GPD).


Variable Documentation#

sl_zigbee_af_green_power_server_generic_switch_commissioning_timeout_event#

sl_zigbee_af_event_t sl_zigbee_af_green_power_server_generic_switch_commissioning_timeout_event

sl_zigbee_af_green_power_server_multi_sensor_commissioning_timeout_event#

sl_zigbee_af_event_t sl_zigbee_af_green_power_server_multi_sensor_commissioning_timeout_event

sl_zigbee_af_green_power_server_commissioning_window_timeout_event#

sl_zigbee_af_event_t sl_zigbee_af_green_power_server_commissioning_window_timeout_event

Function Documentation#

sl_zigbee_af_green_power_server_generic_switch_commissioning_timeout_event_handler#

void sl_zigbee_af_green_power_server_generic_switch_commissioning_timeout_event_handler (sl_zigbee_af_event_t * event)
Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_event_t *N/Aevent

sl_zigbee_af_green_power_server_multi_sensor_commissioning_timeout_event_handler#

void sl_zigbee_af_green_power_server_multi_sensor_commissioning_timeout_event_handler (sl_zigbee_af_event_t * event)
Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_event_t *N/Aevent

sl_zigbee_af_green_power_server_commissioning_window_timeout_event_handler#

void sl_zigbee_af_green_power_server_commissioning_window_timeout_event_handler (sl_zigbee_af_event_t * event)
Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_event_t *N/Aevent

Macro Definition Documentation#

SL_ZIGBEE_AF_GREEN_POWER_GP_SHARED_KEY#

#define SL_ZIGBEE_AF_GREEN_POWER_GP_SHARED_KEY
Value:
0

SL_ZIGBEE_AF_GREEN_POWER_GP_INDIVIDUAL_KEY#

#define SL_ZIGBEE_AF_GREEN_POWER_GP_INDIVIDUAL_KEY
Value:
1

GREEN_POWER_SERVER_GPS_SECURITY_LEVEL_ATTRIBUTE_FIELD_INVOLVE_TC#

#define GREEN_POWER_SERVER_GPS_SECURITY_LEVEL_ATTRIBUTE_FIELD_INVOLVE_TC
Value:
0x08

GP_DEVICE_ANNOUNCE_SIZE#

#define GP_DEVICE_ANNOUNCE_SIZE
Value:
12

SIZE_OF_REPORT_STORAGE#

#define SIZE_OF_REPORT_STORAGE
Value:
82

COMM_REPLY_PAYLOAD_SIZE#

#define COMM_REPLY_PAYLOAD_SIZE
Value:
30

GP_SINK_TABLE_RESPONSE_ENTRIES_OFFSET#

#define GP_SINK_TABLE_RESPONSE_ENTRIES_OFFSET
Value:
(3)

SL_ZIGBEE_AF_ZCL_CLUSTER_GP_GPS_COMMISSIONING_WINDOWS_DEFAULT_TIME_S#

#define SL_ZIGBEE_AF_ZCL_CLUSTER_GP_GPS_COMMISSIONING_WINDOWS_DEFAULT_TIME_S
Value:
(180)

GP_ADDR_SRC_ID_WILDCARD#

#define GP_ADDR_SRC_ID_WILDCARD
Value:
(0xFFFFFFFF)

GPS_ATTRIBUTE_KEY_TYPE_MASK#

#define GPS_ATTRIBUTE_KEY_TYPE_MASK
Value:
(0x07)

GP_PAIRING_CONFIGURATION_FIXED_FLAG#

#define GP_PAIRING_CONFIGURATION_FIXED_FLAG
Value:
(0x230)

GREEN_POWER_SERVER_MIN_REPORT_LENGTH#

#define GREEN_POWER_SERVER_MIN_REPORT_LENGTH
Value:
(10)

FIX_SHIFT_REPORTING_DATA_POSITION_CONVERT_TO_PAYLOAD_INDEX#

#define FIX_SHIFT_REPORTING_DATA_POSITION_CONVERT_TO_PAYLOAD_INDEX
Value:
(3)

CAR_DATA_POINT_OFFSET#

#define CAR_DATA_POINT_OFFSET
Value:
1

GP_DEFAULT_LINK_KEY#

#define GP_DEFAULT_LINK_KEY
Value:
{ 0x5A, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6C, 0x6C, 0x69, 0x61, 0x6E, 0x63, 0x65, 0x30, 0x39 }

genericSwitchCommissioningTimeout#

#define genericSwitchCommissioningTimeout
Value:
(&sl_zigbee_af_green_power_server_generic_switch_commissioning_timeout_event)

multiSensorCommissioningTimeout#

#define multiSensorCommissioningTimeout
Value:
(&sl_zigbee_af_green_power_server_multi_sensor_commissioning_timeout_event)

commissioningWindowTimeout#

#define commissioningWindowTimeout
Value:
(&sl_zigbee_af_green_power_server_commissioning_window_timeout_event)