Network Find#

API and Callbacks for the Network Find Component.

NOTE: This component is deprecated in Zigbee 3.0, but is still used for Zigbee Smart Energy requirements. See the Network Creator and Network Steering components instead for Zigbee 3.0-compliant implementations of this behavior. This component provides legacy Zigbee Home Automation (pre-3.0) implementation of routines for finding and joining any viable network via scanning, rather than joining a specific network. If the application will be deployed in an environment with potentially a lot of open networks, consider implementing a mechanism for network deny listing. Network deny listing may be accomplished by implementing the sl_zigbee_af_network_find_join_cb. To extend the functionality to sub-GHz channels, also enable the Network Find (Sub-GHz) component.

Modules#

Network Find

API#

sl_zigbee_af_set_form_and_join_channel_mask(uint8_t page, uint32_t mask)

Set the channel mask for "find unused" and "find joinable". Permitted pages are 0 and, if Sub-GHz channels are included, then also 28-31.

uint32_t
sl_zigbee_af_form_and_join_get_channel_mask(uint8_t page, bool allChannels)

Return All or preferred channel mask for a given page.

Set the search mode for "find unused" and "find joinable". Mode is a bitmask. Permitted values are set by the FIND_AND_JOIN_MODE_... macros.

uint8_t

Return the current search mode.

#define

Return the preferred channel mask for a given page. Only the bottom 27 bits can be set. The top 5 bits are reserved for the page number and are always zero in a returned channel mask. That leaves the value 0xFFFFFFFF free to indicate an invalid page error.

API Documentation#

sl_zigbee_af_set_form_and_join_channel_mask#

sl_status_t sl_zigbee_af_set_form_and_join_channel_mask (uint8_t page, uint32_t mask)

Set the channel mask for "find unused" and "find joinable". Permitted pages are 0 and, if Sub-GHz channels are included, then also 28-31.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Apage
uint32_tN/Amask

sl_zigbee_af_form_and_join_get_channel_mask#

uint32_t sl_zigbee_af_form_and_join_get_channel_mask (uint8_t page, bool allChannels)

Return All or preferred channel mask for a given page.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Apage

The page to retrieve channel mask

boolN/AallChannels

All or preferred channel mask

Only the bottom 27 bits can be set. The top 5 bits are reserved for the page number and are always zero in a returned channel mask. That leaves the value 0xFFFFFFFF free to indicate an invalid page error.


sl_zigbee_af_set_form_and_join_search_mode#

sl_status_t sl_zigbee_af_set_form_and_join_search_mode (uint8_t mode)

Set the search mode for "find unused" and "find joinable". Mode is a bitmask. Permitted values are set by the FIND_AND_JOIN_MODE_... macros.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Amode

sl_zigbee_af_get_form_and_join_search_mode#

uint8_t sl_zigbee_af_get_form_and_join_search_mode (void )

Return the current search mode.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_zigbee_af_get_form_and_join_channel_mask#

#define sl_zigbee_af_get_form_and_join_channel_mask
Value:
(page)

Return the preferred channel mask for a given page. Only the bottom 27 bits can be set. The top 5 bits are reserved for the page number and are always zero in a returned channel mask. That leaves the value 0xFFFFFFFF free to indicate an invalid page error.