Key Establishment Client/Server#

API and Callbacks for the Key Establishment Cluster Client/Server Component.

Silicon Labs implementation of the Smart Energy Key Establishment cluster. The key establishment cluster is used by the Smart Energy profile to perform Certificate-Based Key Establishment (CBKE), which performs mutual authentication and establishes a symmetric APS link key. Direct CBKE between any two non-TC devices is supported after the two devices have completed partner link key exchange via Trust Center. This component defaults to using CBKE functions with the 163k ECC curve support, but users can also choose the 283k1 ECC curve by selecting the 'CBKE 283k1' component.

API#

bool
checkIssuer(uint8_t *issuer)
void
cleanupAndStopWithDelay(sl_zigbee_af_key_establishment_notify_message_t message, uint8_t delayInSec)
void
sendNextKeyEstablishMessage(sli_zigbee_key_establish_message_t message, uint8_t *data)

Enumerations#

enum
NO_KEY_ESTABLISHMENT_EVENT = 0
CHECK_SUPPORTED_CURVES = 1
BEGIN_KEY_ESTABLISHMENT = 2
GENERATE_KEYS = 3
SEND_EPHEMERAL_DATA_MESSAGE = 4
GENERATE_SHARED_SECRET = 5
SEND_CONFIRM_KEY_MESSAGE = 6
INITIATOR_RECEIVED_CONFIRM_KEY = 7
}

Macros#

#define
EM_AF_KE_INITIATE_SIZE (2 + 1 + 1 + SL_ZIGBEE_CERTIFICATE_SIZE)

Init - bytes: suite (2), key gen time (1), derive secret time (1), cert (48)

#define
EM_AF_KE_INITIATE_SIZE_283K1 (2 + 1 + 1 + SL_ZIGBEE_CERTIFICATE_283K1_SIZE)
#define
EM_AF_KE_EPHEMERAL_SIZE SL_ZIGBEE_PUBLIC_KEY_SIZE
#define
EM_AF_KE_EPHEMERAL_SIZE_283K1 SL_ZIGBEE_PUBLIC_KEY_283K1_SIZE
#define
EM_AF_KE_SMAC_SIZE SL_ZIGBEE_SMAC_SIZE
#define

Terminate - bytes: status (1), wait time (1), suite (2)

#define

The offset within the 163k1 curve certificate struct where the issuer field lives. 22-bytes for Public Key Reconstruction data, and 8-bytes for subject.

#define
CERT_ISSUER_OFFSET (CERT_SUBJECT_OFFSET + 8)
#define
CERT_SUBJECT_OFFSET_283K1 (1 + 8 + 1 + 1 + 8 + 5 + 4)

The offset within the 283k1 curve certificate struct where the issuer field lives. 22-bytes for Public Key Reconstruction data, and 8-bytes for subject.

#define
CERT_ISSUER_OFFSET_283K1 (1 + 8 + 1 + 1)
#define
DEFAULT_EPHEMERAL_DATA_GENERATE_TIME_SECONDS (10 + APS_ACK_TIMEOUT_SECONDS)

These values reported to the remote device as to how long the local device takes to execute these operations.

#define
DEFAULT_GENERATE_SHARED_SECRET_TIME_SECONDS (15 + APS_ACK_TIMEOUT_SECONDS)
#define
sli_zigbee_af_key_establishment_generate_cbke_keys_handler sli_zigbee_af_generate_cbke_keys_callback
#define
sli_zigbee_af_key_establishment_calculate_smacs_handler sli_zigbee_af_calculate_smacs_callback
#define
sli_zigbee_af_key_establishment_generate_cbke_keys_handler283k1 sli_zigbee_af_generate_cbke_keys_callback_283k1
#define
sli_zigbee_af_key_establishment_calculate_smacs_handler283k1 sli_zigbee_af_calculate_smacs_callback_283k1
#define
#define
cleanupAndStop (message)

API Documentation#

checkIssuer#

bool checkIssuer (uint8_t * issuer)
Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Aissuer

cleanupAndStopWithDelay#

void cleanupAndStopWithDelay (sl_zigbee_af_key_establishment_notify_message_t message, uint8_t delayInSec)
Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_key_establishment_notify_message_tN/Amessage
uint8_tN/AdelayInSec

sendCertificate#

sl_zigbee_af_key_establishment_notify_message_t sendCertificate (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

sendNextKeyEstablishMessage#

void sendNextKeyEstablishMessage (sli_zigbee_key_establish_message_t message, uint8_t * data)
Parameters
TypeDirectionArgument NameDescription
sli_zigbee_key_establish_message_tN/Amessage
uint8_t *N/Adata

Enumeration Documentation#

sli_zigbee_key_establish_event_t#

sli_zigbee_key_establish_event_t
Enumerator
NO_KEY_ESTABLISHMENT_EVENT
CHECK_SUPPORTED_CURVES
BEGIN_KEY_ESTABLISHMENT
GENERATE_KEYS
SEND_EPHEMERAL_DATA_MESSAGE
GENERATE_SHARED_SECRET
SEND_CONFIRM_KEY_MESSAGE
INITIATOR_RECEIVED_CONFIRM_KEY

Typedef Documentation#

sli_zigbee_key_establish_message_t#

typedef uint8_t sli_zigbee_key_establish_message_t

Variable Documentation#

sli_zigbee_af_key_establish_message_to_data_size#

const uint8_t sli_zigbee_af_key_establish_message_to_data_size[]

sli_zigbee_af_available_cbke_suite#

sl_zigbee_af_cbke_key_establishment_suite_t sli_zigbee_af_available_cbke_suite

sli_zigbee_af_current_cbke_suite#

sl_zigbee_af_cbke_key_establishment_suite_t sli_zigbee_af_current_cbke_suite

sl_zigbee_af_key_establishment_aps_duplicate_detection_event#

sl_zigbee_af_event_t sl_zigbee_af_key_establishment_aps_duplicate_detection_event

Macro Definition Documentation#

EM_AF_KE_INITIATE_SIZE#

#define EM_AF_KE_INITIATE_SIZE
Value:
(2 + 1 + 1 + SL_ZIGBEE_CERTIFICATE_SIZE)

Init - bytes: suite (2), key gen time (1), derive secret time (1), cert (48)


EM_AF_KE_INITIATE_SIZE_283K1#

#define EM_AF_KE_INITIATE_SIZE_283K1
Value:
(2 + 1 + 1 + SL_ZIGBEE_CERTIFICATE_283K1_SIZE)

EM_AF_KE_EPHEMERAL_SIZE#

#define EM_AF_KE_EPHEMERAL_SIZE
Value:
SL_ZIGBEE_PUBLIC_KEY_SIZE

EM_AF_KE_EPHEMERAL_SIZE_283K1#

#define EM_AF_KE_EPHEMERAL_SIZE_283K1
Value:
SL_ZIGBEE_PUBLIC_KEY_283K1_SIZE

EM_AF_KE_SMAC_SIZE#

#define EM_AF_KE_SMAC_SIZE
Value:
SL_ZIGBEE_SMAC_SIZE

EM_AF_KE_TERMINATE_SIZE#

#define EM_AF_KE_TERMINATE_SIZE
Value:
(1 + 1 + 2)

Terminate - bytes: status (1), wait time (1), suite (2)


APS_ACK_TIMEOUT_SECONDS#

#define APS_ACK_TIMEOUT_SECONDS
Value:
1

KEY_ESTABLISHMENT_APS_DUPLICATE_DETECTION_TIMEOUT_SEC#

#define KEY_ESTABLISHMENT_APS_DUPLICATE_DETECTION_TIMEOUT_SEC
Value:
5

CERT_SUBJECT_OFFSET#

#define CERT_SUBJECT_OFFSET
Value:
22

The offset within the 163k1 curve certificate struct where the issuer field lives. 22-bytes for Public Key Reconstruction data, and 8-bytes for subject.


CERT_ISSUER_OFFSET#

#define CERT_ISSUER_OFFSET
Value:
(CERT_SUBJECT_OFFSET + 8)

CERT_ISSUER_SIZE#

#define CERT_ISSUER_SIZE
Value:
8

CERT_SUBJECT_OFFSET_283K1#

#define CERT_SUBJECT_OFFSET_283K1
Value:
(1 + 8 + 1 + 1 + 8 + 5 + 4)

The offset within the 283k1 curve certificate struct where the issuer field lives. 22-bytes for Public Key Reconstruction data, and 8-bytes for subject.


CERT_ISSUER_OFFSET_283K1#

#define CERT_ISSUER_OFFSET_283K1
Value:
(1 + 8 + 1 + 1)

DEFAULT_EPHEMERAL_DATA_GENERATE_TIME_SECONDS#

#define DEFAULT_EPHEMERAL_DATA_GENERATE_TIME_SECONDS
Value:
(10 + APS_ACK_TIMEOUT_SECONDS)

These values reported to the remote device as to how long the local device takes to execute these operations.


DEFAULT_GENERATE_SHARED_SECRET_TIME_SECONDS#

#define DEFAULT_GENERATE_SHARED_SECRET_TIME_SECONDS
Value:
(15 + APS_ACK_TIMEOUT_SECONDS)

sli_zigbee_af_key_establishment_generate_cbke_keys_handler#

#define sli_zigbee_af_key_establishment_generate_cbke_keys_handler
Value:
sli_zigbee_af_generate_cbke_keys_callback

sli_zigbee_af_key_establishment_calculate_smacs_handler#

#define sli_zigbee_af_key_establishment_calculate_smacs_handler
Value:
sli_zigbee_af_calculate_smacs_callback

sli_zigbee_af_key_establishment_generate_cbke_keys_handler283k1#

#define sli_zigbee_af_key_establishment_generate_cbke_keys_handler283k1
Value:
sli_zigbee_af_generate_cbke_keys_callback_283k1

sli_zigbee_af_key_establishment_calculate_smacs_handler283k1#

#define sli_zigbee_af_key_establishment_calculate_smacs_handler283k1
Value:
sli_zigbee_af_calculate_smacs_callback_283k1

TERMINATE_STATUS_STRINGS#

#define TERMINATE_STATUS_STRINGS
Value:
{ \
"Success", \
"Unknown Issuer", \
"Bad Key Confirm", \
"Bad Message", \
"No resources", \
"Unsupported suite", \
"Invalid certificate", \
"???", \
}

UNKNOWN_TERMINATE_STATUS#

#define UNKNOWN_TERMINATE_STATUS
Value:
7

isCbkeKeyEstablishmentSuiteValid#

#define isCbkeKeyEstablishmentSuiteValid
Value:
()

isCbkeKeyEstablishmentSuite163k1#

#define isCbkeKeyEstablishmentSuite163k1
Value:
(sli_zigbee_af_current_cbke_suite \
== SL_ZIGBEE_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1)

isCbkeKeyEstablishmentSuite283k1#

#define isCbkeKeyEstablishmentSuite283k1
Value:
(sli_zigbee_af_current_cbke_suite \
== SL_ZIGBEE_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1)

cleanupAndStop#

#define cleanupAndStop
Value:
(message)