Manufacturing Library#

API and Callbacks for the Manufacturing Library Component.

This is a manufacturing and functional test library for testing and verifying the RF component of products at manufacture time.

Developers can optionally include this library in their application code. The goal is that in most cases, developers won't need to load multiple images into their hardware at manufacturing time.

This library can optionally be compiled into the developer's production code and run at manufacturing time. Any interface to the library is handled by the application.

This library cannot assist in hardware start up.

Many functions in this file return an sl_status_t value.

API#

typedef void(*
MfglibRxCallback)(uint8_t *packet, uint8_t linkQuality, int8_t rssi)

callback function pointer type for mfglibStart

mfglibStart(MfglibRxCallback mfglibRxCallback)

Activate use of mfglib test routines and enable the radio receiver to report packets it receives to the caller-specified ::mfglibRxCallback() routine.

mfglibEnd(void)

Deactivate use of Manufacturing Library test routines.

Start transmitting the tone feature of the radio.

Stop transmitting a tone started by mfglibStartTone().

Start transmitting a random stream of characters to enable the measurement of radio modulation.

Stop transmitting a random stream of characters started by mfglibStartStream().

mfglibSendPacket(uint8_t *packet, uint16_t repeat)

Send a single packet, (repeat + 1) times.

mfglibSetChannel(uint8_t chan)

Select the radio channel. The channel range is from 11 to 26.

uint8_t

Return the current radio channel, as previously set via mfglibSetChannel().

mfglibSetPower(uint16_t txPowerMode, int8_t power)

First select the transmit power mode, then include a method for selecting the radio transmit power.

int8_t

Return the current radio power setting as previously set via mfglibSetPower().

mfglibSetOptions(uint8_t options)

Set manufacturing library options.

uint8_t

Return the current manufacturing library options, as previously set via mfglibSetOptions().

void
mfglibSetSynOffset(int8_t synOffset)

Set the synth offset in steps.

int8_t

Get the current synth offset in steps.

mfglibSetCtune(uint16_t ctune)

Change the CTUNE value.

uint16_t

Return the current CTUNE value, as previously set via mfglibSetCtune().

#define
mfglibApiStart (packet, linkQuality, rssi)

callback function pointer type for mfglibStart

API Documentation#

MfglibRxCallback#

typedef void(* MfglibRxCallback) (uint8_t *packet, uint8_t linkQuality, int8_t rssi) )(uint8_t *packet, uint8_t linkQuality, int8_t rssi)

callback function pointer type for mfglibStart

Parameters
TypeDirectionArgument NameDescription
[out]packet

pointer to packet data

[out]linkQuality

the calculated link quality measure

[out]rssi

the measured signal strength


mfglibStart#

sl_status_t mfglibStart (MfglibRxCallback mfglibRxCallback)

Activate use of mfglib test routines and enable the radio receiver to report packets it receives to the caller-specified ::mfglibRxCallback() routine.

Parameters
TypeDirectionArgument NameDescription
MfglibRxCallback[in]mfglibRxCallback

A function pointer to callback routine that is invoked whenever a valid packet is received. sl_zigbee_tick() must be called routinely for this callback to function correctly.

It is legal to pass in a NULL. These packets will not be passed up with a CRC failure. The first byte of the packet in the callback is the length. All other functions will return an error until mfglibStart() has been called.

Use this function to enter test mode.

Note: This function should only be called shortly after initialization and prior to forming or joining a network.

Returns


mfglibEnd#

sl_status_t mfglibEnd (void )

Deactivate use of Manufacturing Library test routines.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This restores the hardware to the state it was in prior to mfglibStart() and stops receiving packets started by mfglibStart() at the same time.

Use this function to exit the mfg test mode.

Note: It may be desirable to also reboot after use of manufacturing mode to ensure all application state is properly re-initialized.

Returns


mfglibStartTone#

sl_status_t mfglibStartTone (void )

Start transmitting the tone feature of the radio.

Parameters
TypeDirectionArgument NameDescription
voidN/A

In this mode, the radio will transmit an unmodulated tone on the currently set channel and power level. Upon successful return, the tone will be transmitting. To stop transmitting a tone, the application must call mfglibStopTone(), allowing it the flexibility to determine its own criteria for tone duration, such as time, event, and so on.

Use this function to transmit a tone.

Returns


mfglibStopTone#

sl_status_t mfglibStopTone (void )

Stop transmitting a tone started by mfglibStartTone().

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to stop transmitting a tone.

Returns


mfglibStartStream#

sl_status_t mfglibStartStream (void )

Start transmitting a random stream of characters to enable the measurement of radio modulation.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Enable the measurement of radio modulation.

Returns


mfglibStopStream#

sl_status_t mfglibStopStream (void )

Stop transmitting a random stream of characters started by mfglibStartStream().

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to end the measurement of radio modulation.

Returns


mfglibSendPacket#

sl_status_t mfglibSendPacket (uint8_t * packet, uint16_t repeat)

Send a single packet, (repeat + 1) times.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[in]packet

A packet to be sent. First byte of the packet is always the length byte, the value of which does not include itself but does include the 16-bit CRC in the length calculation. The CRC gets appended automatically by the radio as it transmits the packet, so the host does not need to provide this as part of packetContents. The total length of packet contents (Length Byte+1) going out the radio should not be >128 or <6 bytes. Note that the packet array should not include the CRC, as this is appended by the radio automatically.

uint16_t[in]repeat

The number of times to repeat sending the packet after having been sent once. A value of 0 means send once and don't repeat.

Use this function to send raw data. Historically, the packet array needed to be 16-bit aligned, but recent platforms now require 32-bit alignment (address a multiple of 4), such that ((((uint16_t)packet) & 3) == 0) holds true. (This is generally done by either declaring packet as a local variable or putting it in a global declaration immediately following the declaration of an uint32_t.)

Returns

  • One of the following:


mfglibSetChannel#

sl_status_t mfglibSetChannel (uint8_t chan)

Select the radio channel. The channel range is from 11 to 26.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chan

Valid values depend upon the radio used.

Customers can set any valid channel they want. Calibration occurs if this is the first time after power up.

Use this function to change channels.

Returns


mfglibGetChannel#

uint8_t mfglibGetChannel (void )

Return the current radio channel, as previously set via mfglibSetChannel().

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to get current channel.

Returns

  • Current channel.


mfglibSetPower#

sl_status_t mfglibSetPower (uint16_t txPowerMode, int8_t power)

First select the transmit power mode, then include a method for selecting the radio transmit power.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]txPowerMode

Boost mode or external PA.

int8_t[in]power

Power in units of dBm, which can be negative.

Valid power settings depend upon the specific radio in use. Silicon Labs radios have discrete power settings, and then requested power is rounded to a valid power setting. The actual power output is available to the caller via mfglibGetPower().

Use this function to adjust the transmit power.

Returns


mfglibGetPower#

int8_t mfglibGetPower (void )

Return the current radio power setting as previously set via mfglibSetPower().

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to get current power setting.

Returns

  • The current power setting.


mfglibSetOptions#

sl_status_t mfglibSetOptions (uint8_t options)

Set manufacturing library options.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]options

bitmask. 0 == non-CSMA transmits, 1 == CSMA transmits

Use this function to set manufacturing library options.

Returns


mfglibGetOptions#

uint8_t mfglibGetOptions (void )

Return the current manufacturing library options, as previously set via mfglibSetOptions().

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to get library options.

Returns

  • Current options based on the current test mode.


mfglibSetSynOffset#

void mfglibSetSynOffset (int8_t synOffset)

Set the synth offset in steps.

Parameters
TypeDirectionArgument NameDescription
int8_t[in]synOffset

The number of steps to offset the carrier frequency (may be negative).

Set the synth offset in 9.375 kHz steps on EFR32. This function does NOT write the new synth offset to the token, it only changes it in memory. It can be changed as many times as preferred, and the setting will be lost when a reset occurs. The value will survive deep sleep, but will not survive a reset, thus it will not take effect in the bootloader. To make the value permanent (and accessible to the bootloader), the TOKEN_MFG_SYNTH_FREQ_OFFSET token must be written using the token API or Simplicity Commander.

Use this function to compensate for tolerances in the crystal oscillator or capacitors. This function does not effect a permanent change; once a preferred offset is found, it must be written to a token using the token API for it to be permanent.


mfglibGetSynOffset#

int8_t mfglibGetSynOffset (void )

Get the current synth offset in steps.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Steps are 9.375 kHz on EFR32. See mfglibSetSynOffset() for details. Returns

  • The synth offset.


mfglibSetCtune#

sl_status_t mfglibSetCtune (uint16_t ctune)

Change the CTUNE value.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]ctune

Valid range of a CTUNE values is between 0x0000 - 0x00FF.

This function will idle the radio if mfglib has been started, then set the CTUNE value as desired. mfglib is then restarted to take effect of this new change.

Use this function to change CTUNE value.

Returns


mfglibGetCtune#

uint16_t mfglibGetCtune (void )

Return the current CTUNE value, as previously set via mfglibSetCtune().

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to get current CTUNE value.

Returns

  • Current CTUNE value. If value is 0xFFFF, CTUNE is not available due to missing mfglib support.


mfglibApiStart#

#define mfglibApiStart
Value:
(packet, linkQuality, rssi)

callback function pointer type for mfglibStart