ZLL Level Control Server#

API and Callbacks for the ZLL Level Control Cluster Server Component.

Silicon Labs implementation of the original Zigbee Light Link profile enhancements to the Level Control server cluster. The component is only intended to assist with debugging, as the implemented callbacks simply parse requests from the Identify client and blink LEDs. Before production, this component should be replaced with code that acts on the requests in an appropriate way. Note that the extensions do not now require Touchlink commissioning to be used, and that the commands may now be required by other device types, such as Lighting and Occupancy.

API Documentation#

sl_zigbee_af_zll_level_control_server_move_to_level_with_on_off_zll_extensions#

sl_zigbee_af_status_t sl_zigbee_af_zll_level_control_server_move_to_level_with_on_off_zll_extensions (const sl_zigbee_af_cluster_command_t * cmd)
Parameters
TypeDirectionArgument NameDescription
const sl_zigbee_af_cluster_command_t *N/Acmd

sl_zigbee_af_zll_level_control_server_ignore_move_to_level_move_step_stop#

bool sl_zigbee_af_zll_level_control_server_ignore_move_to_level_move_step_stop (uint8_t endpoint, uint8_t commandId)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint
uint8_tN/AcommandId

Macro Definition Documentation#

SL_ZIGBEE_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MINIMUM_LEVEL#

#define SL_ZIGBEE_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MINIMUM_LEVEL
Value:
0x01

SL_ZIGBEE_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MAXIMUM_LEVEL#

#define SL_ZIGBEE_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MAXIMUM_LEVEL
Value:
0xFE