Data structure of the friend_queue event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t
uint32_t
uint32_t

Public Attribute Documentation#

netkey_index#

uint16_t sl_btmesh_evt_diagnostic_friend_queue_s::netkey_index

Index of the network key used in friendship


Definition at line 22390 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

lpn#

uint16_t sl_btmesh_evt_diagnostic_friend_queue_s::lpn

LPN address


Definition at line 22391 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

src#

uint16_t sl_btmesh_evt_diagnostic_friend_queue_s::src

Source address of the message


Definition at line 22392 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

dst#

uint16_t sl_btmesh_evt_diagnostic_friend_queue_s::dst

Destination address of the message


Definition at line 22393 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ivi#

uint32_t sl_btmesh_evt_diagnostic_friend_queue_s::ivi

IV index used to secure the message


Definition at line 22394 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

seq#

uint32_t sl_btmesh_evt_diagnostic_friend_queue_s::seq

Sequence number of the message


Definition at line 22395 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h