Data structure of the friendship_terminated event.
Public Attribute Documentation#
netkey_index#
uint16_t sl_btmesh_evt_friend_friendship_terminated_s::netkey_index
Index of the network key used in friendship
Definition at line
7836
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
lpn_address#
uint16_t sl_btmesh_evt_friend_friendship_terminated_s::lpn_address
LPN node address
Definition at line
7837
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
reason#
uint16_t sl_btmesh_evt_friend_friendship_terminated_s::reason
Reason for friendship termination
Definition at line
7838
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h