Data structure of the distribution_status event.
Public Attributes#
uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
uint16_t
uint8_t
uint16_t
uint8_t
uint8_t
uint16_t
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::elem_index
Client model element index
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::server_address
Unicast address of the server
status#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::status
Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned
phase#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::phase
Enum sl_btmesh_fw_dist_client_dist_phase_t. Phase of the Distribution Server
group_address#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::group_address
Distribution group address. Ignore if no distribution is active.
appkey_index#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::appkey_index
Distribution app key index. Ignore if no distribution is active.
distributor_ttl#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::distributor_ttl
TTL used by the Distributor. Ignore if no distribution is active.
timeout_base#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::timeout_base
Timeout Base value used in BLOB Transfer
transfer_mode#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::transfer_mode
Transfer Mode used in BLOB Transfer
apply_immediately#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::apply_immediately
1 if the Update Policy is Verify and Apply, otherwise 0. Ignore if no distribution is active.
fw_list_index#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::fw_list_index
Index of the firmware in the Distributor's Firmware List